<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックReviving a newly opened but seemingly dead FRDM-KL46Z</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252931#M7274</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm hoping to revive a fresh out of the box FRDM-KL46Z board which no longer powers up or is either recognized when I plug it in through the SDA USB port. I doubt I'm the only who's in a similar situation. The board stopped working after about 10 minutes of me opening it for the first time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's the events between opening the box to the point where the board stopped working:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The demo app loaded and executed fine when I first plugged the board. Then I followed the Quick Start Guide's advice and copied a precompiled srec file unto the FAT drive. In my case this was the low_power_demo_freedom.srec file. While copying the file the board's yellow light was blinking. When the copying was done the board stopped blinking and I didn't notice any other reaction from the board. I then followed the guide's advice again and copied the FRDMKL46_Demo_freedom.srec file unto the memory. The board's light blinked while the copying was in progress. When the copying was done the light stopped blinking but the demo app was not running (i.e., the LCD was off and pressing SW1 did not scroll through the demo features). At this point I had two srec files on the FAT drive. The low power app and the out-of-the-box demo. So I deleted them from the FAT drive and recopied the demo but again the app did not execute. I then tried to eject the FAT drive but I noticed Windows 7 would not eject it. So I unplugged it and plugged it back in and tried to copy the lower power demo to no success and again the original demo also to no success. I then unplugged the board and plugged it back in while holding down the reset button so I could look into the SDA_INFO file. Being a newbie I didn't see anything interesting except that the board's light was blinking. I then tried to copy the demo app unto the FAT but again the app did not execute. I tried to eject the board and Windows 7 wouldn't eject it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally (sorry for the long story but it's for the sake of accuracy) I just unplugged the board and plugged it back in. Unfortunately this time the board did not come on and Windows did not recognize it as a FAT drive (or anything at all). Unplugging it and plugging it back in does not solve anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems like the board is either bricked or dead. By the way, I'm using an anti-static arm band so I don't think this is the result of ESD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do embedded systems design for a living so I don't mind any suggestions involving checking the board with multimeters, oscilloscopes, using an external power supply, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance! Any suggestions would be appreciated. I doubt that it is this easy to completely damage the board within 10 minutes of opening the box for the first time :smileywink: So I hope I can bring this little guy back to life!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Sep 2013 19:55:36 GMT</pubDate>
    <dc:creator>carlosmendoza</dc:creator>
    <dc:date>2013-09-26T19:55:36Z</dc:date>
    <item>
      <title>Reviving a newly opened but seemingly dead FRDM-KL46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252931#M7274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm hoping to revive a fresh out of the box FRDM-KL46Z board which no longer powers up or is either recognized when I plug it in through the SDA USB port. I doubt I'm the only who's in a similar situation. The board stopped working after about 10 minutes of me opening it for the first time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's the events between opening the box to the point where the board stopped working:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The demo app loaded and executed fine when I first plugged the board. Then I followed the Quick Start Guide's advice and copied a precompiled srec file unto the FAT drive. In my case this was the low_power_demo_freedom.srec file. While copying the file the board's yellow light was blinking. When the copying was done the board stopped blinking and I didn't notice any other reaction from the board. I then followed the guide's advice again and copied the FRDMKL46_Demo_freedom.srec file unto the memory. The board's light blinked while the copying was in progress. When the copying was done the light stopped blinking but the demo app was not running (i.e., the LCD was off and pressing SW1 did not scroll through the demo features). At this point I had two srec files on the FAT drive. The low power app and the out-of-the-box demo. So I deleted them from the FAT drive and recopied the demo but again the app did not execute. I then tried to eject the FAT drive but I noticed Windows 7 would not eject it. So I unplugged it and plugged it back in and tried to copy the lower power demo to no success and again the original demo also to no success. I then unplugged the board and plugged it back in while holding down the reset button so I could look into the SDA_INFO file. Being a newbie I didn't see anything interesting except that the board's light was blinking. I then tried to copy the demo app unto the FAT but again the app did not execute. I tried to eject the board and Windows 7 wouldn't eject it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally (sorry for the long story but it's for the sake of accuracy) I just unplugged the board and plugged it back in. Unfortunately this time the board did not come on and Windows did not recognize it as a FAT drive (or anything at all). Unplugging it and plugging it back in does not solve anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems like the board is either bricked or dead. By the way, I'm using an anti-static arm band so I don't think this is the result of ESD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do embedded systems design for a living so I don't mind any suggestions involving checking the board with multimeters, oscilloscopes, using an external power supply, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance! Any suggestions would be appreciated. I doubt that it is this easy to completely damage the board within 10 minutes of opening the box for the first time :smileywink: So I hope I can bring this little guy back to life!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2013 19:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252931#M7274</guid>
      <dc:creator>carlosmendoza</dc:creator>
      <dc:date>2013-09-26T19:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: Reviving a newly opened but seemingly dead FRDM-KL46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252932#M7275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm glad you were able to solve the problem Carlos, I'm sure your workaround will be useful for some other people, thanks :smileygrin:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2013 16:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252932#M7275</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-10-01T16:37:55Z</dc:date>
    </item>
    <item>
      <title>Re: Reviving a newly opened but seemingly dead FRDM-KL46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252933#M7276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Pedro, I'll try to post about any other problem/solutions I run into while I get used to developing on the FRDM-KL46Z. This KL46Z board is relatively new so there's not many tutorials online with "baby steps".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also wish that Freescale's sample code matched the instructions on the included PDF. The "hello world" example about the serial port doesn't match what the PDF guide says. They should also include the three most common mistakes people will most likely make while trying the examples. That would save Freescale employees the work of answering the same questions over and over on the forums.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's like Erich Styger says, the dev boards and IDEs that are easier to get used to or transition into are the ones that will become popular with the developer community. So far there's a lack of in-depth tutorials for the KL46Z for people coming in from other backgrounds (FPGA, Android, simpler microcontrollers, ...). It's sad because this KL46Z board is very powerful!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Oct 2013 12:39:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252933#M7276</guid>
      <dc:creator>carlosmendoza</dc:creator>
      <dc:date>2013-10-05T12:39:42Z</dc:date>
    </item>
    <item>
      <title>Re: Reviving a newly opened but seemingly dead FRDM-KL46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252934#M7277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's actually good to read that kind of feedback straight from our customers, I will check with some of my peers if we can make a couple of step by step guides on how to use the most common features of the KL mcu's and post them online, I will keep you posted on this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2013 13:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252934#M7277</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-10-07T13:59:14Z</dc:date>
    </item>
    <item>
      <title>Re: Reviving a newly opened but seemingly dead FRDM-KL46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252935#M7278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Pedro, that would be much appreciated by all of us!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, it seems like the answer I posted has disappeared from this original post. It somehow "branched into another discussion". Here's the link with the answer:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/352678"&gt;Re: Reviving a newly opened but seemingly dead FRDM-KL46Z&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2013 14:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reviving-a-newly-opened-but-seemingly-dead-FRDM-KL46Z/m-p/252935#M7278</guid>
      <dc:creator>carlosmendoza</dc:creator>
      <dc:date>2013-10-07T14:06:55Z</dc:date>
    </item>
  </channel>
</rss>