<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: When to use PLL and FLL in Kinetis KL15? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252277#M7207</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Other than the ranges as mentioned, an FLL is lower power, but is less accurate, and in certain conditions less stable, than a PLL.&lt;/P&gt;&lt;P&gt;The FLL produces an average multiple of the reference and changes between two or more different frequencies,&amp;nbsp; where as the PLL is capable of an exact multiple of the reference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 May 2013 02:52:27 GMT</pubDate>
    <dc:creator>JimDon</dc:creator>
    <dc:date>2013-05-23T02:52:27Z</dc:date>
    <item>
      <title>When to use PLL and FLL in Kinetis KL15?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252274#M7204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using Kinets &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL1x"&gt;KL15&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why is there a PLL and a FLL?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which one should I choose and why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2013 14:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252274#M7204</guid>
      <dc:creator>markosiponen</dc:creator>
      <dc:date>2013-05-22T14:19:22Z</dc:date>
    </item>
    <item>
      <title>Re: When to use PLL and FLL in Kinetis KL15?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252275#M7205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found more restrictions (I think):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;FLL&lt;/STRONG&gt;: is up to 48MHz&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PLL&lt;/STRONG&gt;: is upp to100MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And the PLL draws 600µA at 48MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So If i want MCGOUTCLK at 48MHz, should I prefer to select the FLL instead of the PLL (saving 600µA)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or is there some other benefits of selecting the PLL (not saving 600µA)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2013 14:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252275#M7205</guid>
      <dc:creator>markosiponen</dc:creator>
      <dc:date>2013-05-22T14:52:35Z</dc:date>
    </item>
    <item>
      <title>Re: When to use PLL and FLL in Kinetis KL15?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252276#M7206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Markosiponen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are many clock mode in &lt;A href="http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=KINETIS_L_SERIES"&gt;KL series&lt;/A&gt;, As you kniow, the input source of FLL and PLL are different. PLL source is external clock and FLL can both from internal clock and external clock. The reference clock range are different. FLL reference clock is from 31.25KHz to 39.0625KHz. But PLL reference clock is from 2MHz to 4MHz. So you need to choose PLL and FLL according to your application. You can find chapter 4 clocking system in document "Kinetis L Peripheral Module Quick Reference". You can download this document from link &lt;A href="http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KLQRUG.pdf?fsrch=1&amp;amp;sr=4"&gt;http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KLQRUG.pdf?fsrch=1&amp;amp;sr=4&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2013 01:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252276#M7206</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-05-23T01:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: When to use PLL and FLL in Kinetis KL15?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252277#M7207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Other than the ranges as mentioned, an FLL is lower power, but is less accurate, and in certain conditions less stable, than a PLL.&lt;/P&gt;&lt;P&gt;The FLL produces an average multiple of the reference and changes between two or more different frequencies,&amp;nbsp; where as the PLL is capable of an exact multiple of the reference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2013 02:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252277#M7207</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2013-05-23T02:52:27Z</dc:date>
    </item>
    <item>
      <title>Re: When to use PLL and FLL in Kinetis KL15?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252278#M7208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The answer that was relevant to me is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need the FLL or PLL if you need to run the processor at 48 MHz or faster than the external crystal will run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whether you use the PLL or FLL depends on whether you want low power and to put the unit to sleep and wake up quickly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can run the FLL off of a 32khz crystal. The FLL also comes up faster than the PLL.&lt;/P&gt;&lt;P&gt;The PLL requires a 4MHz reference (I think roughly this is true) And takes longer to stabilize than the FLL.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Nov 2014 23:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-to-use-PLL-and-FLL-in-Kinetis-KL15/m-p/252278#M7208</guid>
      <dc:creator>gibbon1</dc:creator>
      <dc:date>2014-11-14T23:11:04Z</dc:date>
    </item>
  </channel>
</rss>