<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K60 ethernet problem when using FLL in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ethernet-problem-when-using-FLL/m-p/251095#M7096</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a K60 revision 2 and what I'm trying to do is run the chip from the RTC oscillator. I have apparently managed to achieve this, but the problem comes when the ethernet is involved, I set the R flag on a TX buffer to indicate that the K60 should send the frame, and the flag never gets cleared.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a PK60DN512VLK10 2N22D&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board has two clocks, a 50MHz on EXTAL and 32.768KHz on EXTAL32. Prior to the revision 2 it wasn't possible to use the RTC oscillator to drive the FLL so I have been using the 50MHz signal and generating a 96MHz PLL for the core clock, then setting the dividers to get a 48MHz bus and 24MHz flash. I have the dividers the same on the FLL so as far as I know everything is running at the same speed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any issues that I should be aware about when changing from a PLL to FLL? Hypothetically if I did have it running at a slower speed than what the PLL is running at, why would this effect the TX buffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Oct 2013 16:46:52 GMT</pubDate>
    <dc:creator>James8</dc:creator>
    <dc:date>2013-10-31T16:46:52Z</dc:date>
    <item>
      <title>K60 ethernet problem when using FLL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ethernet-problem-when-using-FLL/m-p/251095#M7096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a K60 revision 2 and what I'm trying to do is run the chip from the RTC oscillator. I have apparently managed to achieve this, but the problem comes when the ethernet is involved, I set the R flag on a TX buffer to indicate that the K60 should send the frame, and the flag never gets cleared.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a PK60DN512VLK10 2N22D&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board has two clocks, a 50MHz on EXTAL and 32.768KHz on EXTAL32. Prior to the revision 2 it wasn't possible to use the RTC oscillator to drive the FLL so I have been using the 50MHz signal and generating a 96MHz PLL for the core clock, then setting the dividers to get a 48MHz bus and 24MHz flash. I have the dividers the same on the FLL so as far as I know everything is running at the same speed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any issues that I should be aware about when changing from a PLL to FLL? Hypothetically if I did have it running at a slower speed than what the PLL is running at, why would this effect the TX buffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2013 16:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ethernet-problem-when-using-FLL/m-p/251095#M7096</guid>
      <dc:creator>James8</dc:creator>
      <dc:date>2013-10-31T16:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: K60 ethernet problem when using FLL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ethernet-problem-when-using-FLL/m-p/251096#M7097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, James&lt;/P&gt;&lt;P&gt;i checked K60 version2 reference manual. I think RTC clock can be provided as source of FLL. You can find this path in figure 5-1 Clocking diagram in reference manual "K60P144M100SF2RM".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2013 03:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ethernet-problem-when-using-FLL/m-p/251096#M7097</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-11-12T03:19:34Z</dc:date>
    </item>
  </channel>
</rss>