<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic My SPI Reading doesn't function. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/My-SPI-Reading-doesn-t-function/m-p/250938#M7073</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Iam using k70. My SPI Reading (first writing like 2 bytes then reading one byte, FIFO function is disabled) doesn't function. I used RFDF and TCF two interrupt sources. But funny is, I could get the right read-value when I set one breakpoint at RFDF-ISR, withoutsetting this breakpoint, I could never get the correct value.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Feb 2014 08:16:39 GMT</pubDate>
    <dc:creator>wangk70</dc:creator>
    <dc:date>2014-02-21T08:16:39Z</dc:date>
    <item>
      <title>My SPI Reading doesn't function.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/My-SPI-Reading-doesn-t-function/m-p/250938#M7073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Iam using k70. My SPI Reading (first writing like 2 bytes then reading one byte, FIFO function is disabled) doesn't function. I used RFDF and TCF two interrupt sources. But funny is, I could get the right read-value when I set one breakpoint at RFDF-ISR, withoutsetting this breakpoint, I could never get the correct value.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2014 08:16:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/My-SPI-Reading-doesn-t-function/m-p/250938#M7073</guid>
      <dc:creator>wangk70</dc:creator>
      <dc:date>2014-02-21T08:16:39Z</dc:date>
    </item>
    <item>
      <title>Re: My SPI Reading doesn't function.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/My-SPI-Reading-doesn-t-function/m-p/250939#M7074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wang,&lt;/P&gt;&lt;P&gt;I've had a brief look through your question and I'm also not sure of the reason that cause the issue.&lt;/P&gt;&lt;P&gt;I wonder if you could show me the data stream figure between the MCU and slave.&lt;/P&gt;&lt;P&gt;I've attached a demo about K60 communicate with a external flash chip and please refer to it for details.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 08:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/My-SPI-Reading-doesn-t-function/m-p/250939#M7074</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-02-25T08:13:32Z</dc:date>
    </item>
  </channel>
</rss>