<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K10 - Crystal design using internal load capacitors in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Crystal-design-using-internal-load-capacitors/m-p/250112#M7017</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Joe&lt;/P&gt;&lt;P&gt;First, crystal loading capacitor value depends on manufacturer specification. If your crystal need loading capacitor is 22pF, you can enable bit SC2P, SC4P and SC16P together. The internal capacitors are paralleled. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jan 2014 07:50:18 GMT</pubDate>
    <dc:creator>Paul_Tian</dc:creator>
    <dc:date>2014-01-23T07:50:18Z</dc:date>
    <item>
      <title>K10 - Crystal design using internal load capacitors</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Crystal-design-using-internal-load-capacitors/m-p/250111#M7016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not finding much information on the design alternatives on using a 4.0 mhz crystal with a K10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The several app notes talk about the danger of using too hi a drive but I can't find any thing that helps determine if my application should be set up as lo drive or hi drive.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The documents also suggest that the external load resistor and caps may not be required by using the internal caps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where can I find information that explores those options so I can decide what's acceptable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The User Guide is very - very weak on this subject and the app notes are too general.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If anyone has insight or direction - please provide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2014 00:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Crystal-design-using-internal-load-capacitors/m-p/250111#M7016</guid>
      <dc:creator>JHinkle</dc:creator>
      <dc:date>2014-01-23T00:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: K10 - Crystal design using internal load capacitors</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Crystal-design-using-internal-load-capacitors/m-p/250112#M7017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Joe&lt;/P&gt;&lt;P&gt;First, crystal loading capacitor value depends on manufacturer specification. If your crystal need loading capacitor is 22pF, you can enable bit SC2P, SC4P and SC16P together. The internal capacitors are paralleled. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2014 07:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Crystal-design-using-internal-load-capacitors/m-p/250112#M7017</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-01-23T07:50:18Z</dc:date>
    </item>
  </channel>
</rss>