<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: SPI problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250008#M7003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your answer. The component I'm using is SPISlave_LDD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jul 2013 06:40:51 GMT</pubDate>
    <dc:creator>josemartinez</dc:creator>
    <dc:date>2013-07-03T06:40:51Z</dc:date>
    <item>
      <title>SPI problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250006#M7001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm triying to use the SPI with kinetis K20, I want to use it as a Slave and other device will be a Master, this device will generate a CLK signal and it will send de data. The CLK is 2 MHz.&lt;/P&gt;&lt;P&gt;I have done the configuration the image shows. I'm not able to receive any data, I don't know why, probably I'm doing something wrong, its the first time I work with kinetis. If some one can help me....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 15:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250006#M7001</guid>
      <dc:creator>josemartinez</dc:creator>
      <dc:date>2013-07-02T15:43:09Z</dc:date>
    </item>
    <item>
      <title>Re: SPI problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250007#M7002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your attached picture, I could not find the SPI mode selected. Which processor expert component you are using? If it is [Init_SPI] component?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 03:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250007#M7002</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-07-03T03:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: SPI problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250008#M7003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your answer. The component I'm using is SPISlave_LDD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 06:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250008#M7003</guid>
      <dc:creator>josemartinez</dc:creator>
      <dc:date>2013-07-03T06:40:51Z</dc:date>
    </item>
    <item>
      <title>Re: SPI problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250009#M7004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have make a demo on TWR-K40X256 boards with [SPISlave_LDD] &amp;amp; [SPIMaster_LDD], which could use TWR-K40X256 J4 jumper.&lt;/P&gt;&lt;P&gt;J4-1 PTA16 SPI0_SOUT (ALT2)&lt;/P&gt;&lt;P&gt;J4-4 PTA15 SPI0_SCK (ALT2)&lt;/P&gt;&lt;P&gt;J4-6 PTA14 SPI0_PCS0 (ALT2)&lt;/P&gt;&lt;P&gt;J4-7 PTA17 SPI0_SIN (ALT2)&lt;/P&gt;&lt;P&gt;J4-8 GND&lt;/P&gt;&lt;P&gt;I also attached my test project for your reference.&lt;/P&gt;&lt;P&gt;Both SPI slave and master can receive the data.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2013 06:54:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250009#M7004</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-07-05T06:54:57Z</dc:date>
    </item>
    <item>
      <title>Re: SPI problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250010#M7005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have the data been ready in the K20 SPI's data register before external master launch the reading operation? I have some customers met such problem due to this, please kindly check it in your application code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2013 06:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250010#M7005</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2013-07-05T06:59:09Z</dc:date>
    </item>
    <item>
      <title>Re: SPI problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250011#M7006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer, I had something wrong in my code, I correct it and now its working well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jose&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2013 15:17:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-problem/m-p/250011#M7006</guid>
      <dc:creator>josemartinez</dc:creator>
      <dc:date>2013-07-26T15:17:22Z</dc:date>
    </item>
  </channel>
</rss>