<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: UART help on K10</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-help-on-K10/m-p/162081#M694</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"The UARTs support 10 and 11 bit characters. That means that they can operate in 8 bit character mode with or without parity but plus one stop bit:&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; start bit, 8 bit character, one stop bit)&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; start bit, 8 bit character, parity bit, one stop bit)&lt;/P&gt;&lt;P&gt;or 7 bit character mode with parity&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; start bit, 7 bit character, parity bit, one stop bit)&lt;/P&gt;&lt;P&gt;In addition an address bit can be used (generally known as multi-drop or 9 bit mode).&lt;/P&gt;&lt;P&gt;&lt;EM&gt;When in 7 bit character mode the parity bit is received as 8th bit in the receive data register and so needs to be masked out in software to avoid corruption.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;This means that there are some restrictions as to what formats are possible since 1.5 or 2 stop bits cannot be configured and also 7 bit character mode without parity is not supported."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Reference: &lt;A href="http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf&lt;/A&gt; (section UARTs).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 12 May 2012 04:04:57 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2012-05-12T04:04:57Z</dc:date>
    <item>
      <title>UART help on K10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-help-on-K10/m-p/162080#M693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Referring to K10 user manual, the UART can work 8 bit,9 bit data bits, but my customer requires 7 bit data bits, 1 bit parity (odd) check, 2 stop bits.&lt;/P&gt;&lt;P&gt;in K10 manual, it can work at 8bit data format, and enable parity bits, it only 7 bits data, but we can't generate 2 bit stop.&lt;/P&gt;&lt;P&gt;Do you have any suggestion?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 May 2012 20:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-help-on-K10/m-p/162080#M693</guid>
      <dc:creator>huaping</dc:creator>
      <dc:date>2012-05-11T20:44:17Z</dc:date>
    </item>
    <item>
      <title>Re: UART help on K10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-help-on-K10/m-p/162081#M694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"The UARTs support 10 and 11 bit characters. That means that they can operate in 8 bit character mode with or without parity but plus one stop bit:&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; start bit, 8 bit character, one stop bit)&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; start bit, 8 bit character, parity bit, one stop bit)&lt;/P&gt;&lt;P&gt;or 7 bit character mode with parity&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; start bit, 7 bit character, parity bit, one stop bit)&lt;/P&gt;&lt;P&gt;In addition an address bit can be used (generally known as multi-drop or 9 bit mode).&lt;/P&gt;&lt;P&gt;&lt;EM&gt;When in 7 bit character mode the parity bit is received as 8th bit in the receive data register and so needs to be masked out in software to avoid corruption.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;This means that there are some restrictions as to what formats are possible since 1.5 or 2 stop bits cannot be configured and also 7 bit character mode without parity is not supported."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Reference: &lt;A href="http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf&lt;/A&gt; (section UARTs).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 May 2012 04:04:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-help-on-K10/m-p/162081#M694</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2012-05-12T04:04:57Z</dc:date>
    </item>
  </channel>
</rss>