<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC DIFFERENTIAL TO SINGLE ENDED CONVERSION in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DIFFERENTIAL-TO-SINGLE-ENDED-CONVERSION/m-p/249018#M6902</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0px 0px 10pt;"&gt;&lt;SPAN style="color: #51626f; line-height: 115%; font-family: 'Times New Roman','serif'; font-size: 12pt;"&gt;On the K10 48 pin microcontroller, pins 7 and 8 are ADC0_DP0 and ADC0_DM0- differential inputs. We are trying to optimize use of single ended inputs. Is there a way to use these pins for single ended inputs? If we set one of these pins to ground, will the other essential become a single ended input? Is there a way to use both of these pins for single ended input?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Feb 2014 16:59:03 GMT</pubDate>
    <dc:creator>cmcc</dc:creator>
    <dc:date>2014-02-20T16:59:03Z</dc:date>
    <item>
      <title>ADC DIFFERENTIAL TO SINGLE ENDED CONVERSION</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DIFFERENTIAL-TO-SINGLE-ENDED-CONVERSION/m-p/249018#M6902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0px 0px 10pt;"&gt;&lt;SPAN style="color: #51626f; line-height: 115%; font-family: 'Times New Roman','serif'; font-size: 12pt;"&gt;On the K10 48 pin microcontroller, pins 7 and 8 are ADC0_DP0 and ADC0_DM0- differential inputs. We are trying to optimize use of single ended inputs. Is there a way to use these pins for single ended inputs? If we set one of these pins to ground, will the other essential become a single ended input? Is there a way to use both of these pins for single ended input?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 16:59:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DIFFERENTIAL-TO-SINGLE-ENDED-CONVERSION/m-p/249018#M6902</guid>
      <dc:creator>cmcc</dc:creator>
      <dc:date>2014-02-20T16:59:03Z</dc:date>
    </item>
    <item>
      <title>Re: ADC DIFFERENTIAL TO SINGLE ENDED CONVERSION</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DIFFERENTIAL-TO-SINGLE-ENDED-CONVERSION/m-p/249019#M6903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to table "3.7.1.3.1.1 ADC0 Channel Assignment for 48-Pin Package" in &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/K10P48M50SF0RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;Parent_nodeId=1326497952624724441957&amp;amp;Parent_pageType=product"&gt;K10P48M50SF0RM&lt;/A&gt;, these inputs are individually valid in 'single-ended' mode, as selections 0 and 19.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Feb 2014 23:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DIFFERENTIAL-TO-SINGLE-ENDED-CONVERSION/m-p/249019#M6903</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2014-02-22T23:21:03Z</dc:date>
    </item>
    <item>
      <title>Re: ADC DIFFERENTIAL TO SINGLE ENDED CONVERSION</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DIFFERENTIAL-TO-SINGLE-ENDED-CONVERSION/m-p/249020#M6904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chris,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are below describtion in K10P48M50SF0RM:&lt;/P&gt;&lt;P&gt;"All DADPx inputs may be used as single-ended inputs if the DIFF bit is low. In certain MCU configurations, some DADMx inputs may also be used as single-ended inputs if the DIFF bit is low. Refer to the Chip Configuration chapter for ADC connections specific to this MCU."&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ADC DM may also.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42810iC63A336CF7A34FCD/image-size/large?v=v2&amp;amp;px=999" role="button" title="ADC DM may also.jpg" alt="ADC DM may also.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ADC single ended.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42811i58ED25BB3EC4851B/image-size/large?v=v2&amp;amp;px=999" role="button" title="ADC single ended.jpg" alt="ADC single ended.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2014 01:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DIFFERENTIAL-TO-SINGLE-ENDED-CONVERSION/m-p/249020#M6904</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2014-02-24T01:34:19Z</dc:date>
    </item>
    <item>
      <title>Re: ADC DIFFERENTIAL TO SINGLE ENDED CONVERSION</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DIFFERENTIAL-TO-SINGLE-ENDED-CONVERSION/m-p/249021#M6905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Primarily, i am beginner in this field, but I&amp;nbsp; have a question about differential mode, specifically about the configuration of registers. I am using a PK60DN512VMD10 core on TWR-K60D100M and I am working in CW 10.3. I want to process data taken from a linescan camera on ADC0 in differential mode. As it is in the table above, for using ADC0_DP0 and ADC0_DM0 in differential mode i need to set ADC0_SC1A_DIFFERENTIAL and put 0x0 value in ADC0_SC1A_ADCH. As I read so far, i understood that only these two things must be configured&amp;nbsp; to get data to be processed by the convertor. Physical ADC0_DM0(J4 ,PIN 9) is grounded and ADC0_DP0 (J4, PIN 8) is connected to AOUT signal of the linescan camera. I made this configuration without any result.&lt;/P&gt;&lt;P&gt;I am not sure that i understand the operation of the convertor and that I need help or a example code if possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mihai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Nov 2014 20:29:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DIFFERENTIAL-TO-SINGLE-ENDED-CONVERSION/m-p/249021#M6905</guid>
      <dc:creator>mihaicoca</dc:creator>
      <dc:date>2014-11-24T20:29:27Z</dc:date>
    </item>
  </channel>
</rss>