<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KE18F512VLH16 ECC RAM Single Bit Correction in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2416735#M68522</link>
    <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237024"&gt;@rseigle77&lt;/a&gt;&amp;nbsp;，&lt;/P&gt;
&lt;P&gt;Thanks for your patience. I got the reply from the internal.&lt;/P&gt;
&lt;P&gt;ECC "correction" means returning corrected data to the CPU, not fixing the underlying bit stored in SRAM. Automatic repair requires a separate scrub/write-back mechanism.&lt;/P&gt;
&lt;P&gt;The recommended flow to use software scrub:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;ECC corrects data on read.&lt;/LI&gt;
&lt;LI&gt;Single-bit error interrupt/status is raised. Refer to RM 6.3.1.1 Determining source of the interrupt. MCM_LMPECR&lt;SPAN class="error"&gt;[ER1BR]&lt;/SPAN&gt;=1&lt;/LI&gt;
&lt;LI&gt;Software reads the fault address. MCM_LMPEIR&lt;SPAN class="error"&gt;[PEELOC]&lt;/SPAN&gt; = 5'h08 - a 1-bit correctable ECC event from SRAM_L, MCM_LMFAR indicates fault address.&lt;/LI&gt;
&lt;LI&gt;Software rewrites the corrected value back to the same address.&lt;/LI&gt;
&lt;LI&gt;New ECC syndrome is generated and stored.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
    <pubDate>Mon, 28 Sep 2026 10:25:44 GMT</pubDate>
    <dc:creator>Celeste_Liu</dc:creator>
    <dc:date>2026-09-28T10:25:44Z</dc:date>
    <item>
      <title>KE18F512VLH16 ECC RAM Single Bit Correction</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2404369#M68466</link>
      <description>&lt;P&gt;I have a follow up question related to&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/90401"&gt;@sean_dvorscak&lt;/a&gt;'s post the other day (&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/KE1-ECC-RAM-Single-Bit-Corrrection/m-p/2399360#M68449" target="_blank"&gt;KE1 ECC RAM Single Bit Corrrection&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237877"&gt;@Celeste_Liu&lt;/a&gt;&amp;nbsp;replied,&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;&amp;gt;&amp;nbsp;If implementing an optional scrub, please align the access according to the actual access size or scrub granularity, not blindly to the raw MCM_LMFAR value. Also don't use a fixed 4-byte access unless you first align the address appropriately and confirm the access size is valid.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can&amp;nbsp;MCM_LMFATR[PEFSIZE] be used to determine the access size? If so, can this be used in tandem with&amp;nbsp;MCM_LMFAR to implement a&amp;nbsp;read-correct-writeback operation? For example, if&amp;nbsp;MCM_LMFATR[PEFSIZE] is 3'b000 indicating an 8-bit access, can I perform an 8-bit read from the address indicated by&amp;nbsp;MCM_LMFAR then perform an 8-bit write to the same address to correct the error. Similarly, if&amp;nbsp;MCM_LMFATR[PEFSIZE] is 3'b010 indicating a 32-bit access, can I perform a 32-bit write to the address indicated by MCM_LMFAR without worrying about alignment?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Aug 2026 00:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2404369#M68466</guid>
      <dc:creator>rseigle77</dc:creator>
      <dc:date>2026-08-13T00:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F512VLH16 ECC RAM Single Bit Correction</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2406179#M68482</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237024"&gt;@rseigle77&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I have seen your post. Let me spend some time investigating this issue, and I will get back to you once I have more information.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Tue, 18 Aug 2026 11:16:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2406179#M68482</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-08-18T11:16:22Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F512VLH16 ECC RAM Single Bit Correction</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2406512#M68483</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237024"&gt;@rseigle77&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Regarding your question, I need to escalate it to our internal team for further investigation. According to our process, please provide the &lt;STRONG&gt;end application&lt;/STRONG&gt; name.&lt;/P&gt;
&lt;P&gt;Thanks for your cooperation.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Wed, 19 Aug 2026 09:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2406512#M68483</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-08-19T09:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F512VLH16 ECC RAM Single Bit Correction</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2406684#M68484</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237877"&gt;@Celeste_Liu&lt;/a&gt;&amp;nbsp; - P7 is the name of the end application.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Aug 2026 16:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2406684#M68484</guid>
      <dc:creator>rseigle77</dc:creator>
      <dc:date>2026-08-19T16:54:15Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F512VLH16 ECC RAM Single Bit Correction</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2413807#M68509</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237877"&gt;@Celeste_Liu&lt;/a&gt;, is there any update on this?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2026 22:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2413807#M68509</guid>
      <dc:creator>rseigle77</dc:creator>
      <dc:date>2026-09-15T22:45:05Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F512VLH16 ECC RAM Single Bit Correction</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2415952#M68520</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237024"&gt;@rseigle77&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Sorry, I still haven't received a response from the internal yet.&lt;/P&gt;
&lt;P&gt;I'll follow up with them again and make this my top priority. As soon as I hear anything back, I'll let you know right away.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2026 09:18:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2415952#M68520</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-09-24T09:18:14Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F512VLH16 ECC RAM Single Bit Correction</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2416735#M68522</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237024"&gt;@rseigle77&lt;/a&gt;&amp;nbsp;，&lt;/P&gt;
&lt;P&gt;Thanks for your patience. I got the reply from the internal.&lt;/P&gt;
&lt;P&gt;ECC "correction" means returning corrected data to the CPU, not fixing the underlying bit stored in SRAM. Automatic repair requires a separate scrub/write-back mechanism.&lt;/P&gt;
&lt;P&gt;The recommended flow to use software scrub:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;ECC corrects data on read.&lt;/LI&gt;
&lt;LI&gt;Single-bit error interrupt/status is raised. Refer to RM 6.3.1.1 Determining source of the interrupt. MCM_LMPECR&lt;SPAN class="error"&gt;[ER1BR]&lt;/SPAN&gt;=1&lt;/LI&gt;
&lt;LI&gt;Software reads the fault address. MCM_LMPEIR&lt;SPAN class="error"&gt;[PEELOC]&lt;/SPAN&gt; = 5'h08 - a 1-bit correctable ECC event from SRAM_L, MCM_LMFAR indicates fault address.&lt;/LI&gt;
&lt;LI&gt;Software rewrites the corrected value back to the same address.&lt;/LI&gt;
&lt;LI&gt;New ECC syndrome is generated and stored.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Mon, 28 Sep 2026 10:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2416735#M68522</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-09-28T10:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F512VLH16 ECC RAM Single Bit Correction</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2416871#M68525</link>
      <description>&lt;P&gt;Thanks for the response&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237877"&gt;@Celeste_Liu&lt;/a&gt;,&amp;nbsp;but that does not answer my question regarding &lt;SPAN&gt;MCM_LMFATR[PEFSIZE]&lt;/SPAN&gt;:&lt;/P&gt;&lt;P&gt;"&lt;SPAN&gt;Can&amp;nbsp;MCM_LMFATR[PEFSIZE] be used to determine the access size? If so, can this be used in tandem with&amp;nbsp;MCM_LMFAR to implement a&amp;nbsp;read-correct-writeback operation? For example, if&amp;nbsp;MCM_LMFATR[PEFSIZE] is 3'b000 indicating an 8-bit access, can I perform an 8-bit read from the address indicated by&amp;nbsp;MCM_LMFAR then perform an 8-bit write to the same address to correct the error. Similarly, if&amp;nbsp;MCM_LMFATR[PEFSIZE] is 3'b010 indicating a 32-bit access, can I perform a 32-bit write to the address indicated by MCM_LMFAR without worrying about alignment?"&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Sep 2026 22:37:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-RAM-Single-Bit-Correction/m-p/2416871#M68525</guid>
      <dc:creator>rseigle77</dc:creator>
      <dc:date>2026-09-28T22:37:38Z</dc:date>
    </item>
  </channel>
</rss>