<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KW45B41Z EVK not programming over on board Debugger MCU Link.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45B41Z-EVK-not-programming-over-on-board-Debugger-MCU-Link/m-p/2415672#M68519</link>
    <description>&lt;P&gt;Since the Secure Provisioning Tool can successfully flash and run code on the chip, the physical hardware is completely fine, meaning the "0 SWD Devices detected" error stems from a communication mismatch between your IDE's debug probe server and the onboard MCU-Link firmware. This is usually resolved by updating the MCU-Link firmware to the latest version compatible with your IDE, or by manually holding down the reset button during the connection sequence to prevent a low-power application state from locking out the debug interface.&lt;/P&gt;</description>
    <pubDate>Wed, 23 Sep 2026 10:00:01 GMT</pubDate>
    <dc:creator>craig15miller</dc:creator>
    <dc:date>2026-09-23T10:00:01Z</dc:date>
    <item>
      <title>KW45B41Z EVK not programming over on board Debugger MCU Link.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45B41Z-EVK-not-programming-over-on-board-Debugger-MCU-Link/m-p/2398068#M68439</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P class=""&gt;I am trying to program the &lt;STRONG&gt;KW45B41Z-EVK&lt;/STRONG&gt; using the &lt;STRONG&gt;kw45b41zevk_hello_world&lt;/STRONG&gt; SDK example code. When I start debugging, the onboard debugger gets detected, but then I get the following error:&lt;/P&gt;&lt;P class=""&gt;&lt;STRONG&gt;0 Available SWD Devices detected.&lt;BR /&gt;&lt;STRONG&gt;Connect a device and try again.&lt;/STRONG&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have connected the USB cable to &lt;STRONG&gt;J14&lt;/STRONG&gt; and left &lt;STRONG&gt;JP22 open&lt;/STRONG&gt; (to program using the onboard debugger itself). Also, &lt;STRONG&gt;JP28 pins 1 and 2 are shorted&lt;/STRONG&gt;, as mentioned in the &lt;STRONG&gt;KW45UM&lt;/STRONG&gt;. However, even after that, I am unable to program and debug the example.&lt;/P&gt;&lt;P&gt;I have also tried the &lt;STRONG&gt;kw45b41zevk_led_blinky&lt;/STRONG&gt; SDK example, but it behaves in the same way.&lt;/P&gt;&lt;P&gt;I also tried using an external debugger to debug the board by shorting &lt;STRONG&gt;JP22&lt;/STRONG&gt;, as mentioned in the &lt;STRONG&gt;KW45UM&lt;/STRONG&gt;, but I am getting the same issue.&lt;/P&gt;&lt;P&gt;I have attached a screenshot of the issue I am facing.&lt;/P&gt;&lt;P class=""&gt;I also tried to erase the flash and write the image using the &lt;STRONG&gt;Secure Provisioning Tool&lt;/STRONG&gt;. First, I entered ISP mode by shorting &lt;STRONG&gt;JP25&lt;/STRONG&gt; to enable &lt;STRONG&gt;SW4&lt;/STRONG&gt;, then long-pressed &lt;STRONG&gt;SW4&lt;/STRONG&gt; and &lt;STRONG&gt;Reset (SW3)&lt;/STRONG&gt;. Once the &lt;STRONG&gt;Test Connection&lt;/STRONG&gt; passed, I erased the flash (location &lt;STRONG&gt;0x00000000&lt;/STRONG&gt;, size &lt;STRONG&gt;0x100000&lt;/STRONG&gt;) successfully. Then I used the following image:&lt;/P&gt;&lt;P&gt;${SPT_INSTALL_BIN}\data\sample_data\targets\KW45B41Z8\source_images\kw45b41zevk_led_blinky.s19&lt;/P&gt;&lt;P&gt;I was able to build and program the image successfully, and the intended &lt;STRONG&gt;RGB LED1&lt;/STRONG&gt; is also blinking indicating that KW45B41Z microcontroller is working fine. However, even after this, I am still unable to program or debug the board.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jul 2026 07:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45B41Z-EVK-not-programming-over-on-board-Debugger-MCU-Link/m-p/2398068#M68439</guid>
      <dc:creator>kaif1</dc:creator>
      <dc:date>2026-07-23T07:01:24Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z EVK not programming over on board Debugger MCU Link.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45B41Z-EVK-not-programming-over-on-board-Debugger-MCU-Link/m-p/2398717#M68443</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250524"&gt;@kaif1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which IDE are you using?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;MCUXpresso IDE or MCUXpresso for VS Code?&lt;/P&gt;
&lt;P&gt;Let me have a try on my side, then let you know the default jumper settings.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Christine.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jul 2026 10:26:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45B41Z-EVK-not-programming-over-on-board-Debugger-MCU-Link/m-p/2398717#M68443</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2026-07-24T10:26:12Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z EVK not programming over on board Debugger MCU Link.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45B41Z-EVK-not-programming-over-on-board-Debugger-MCU-Link/m-p/2399821#M68452</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250524"&gt;@kaif1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to my jumper settings, and I verified on my local side, I can flash hello_world example into the board successfully.&lt;/P&gt;
&lt;P&gt;And I am using MCUXpresso IDE with SDK 25.12.00.&lt;/P&gt;
&lt;P&gt;Please have a try with my jumper settings and then let me know whether it works for you .&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Christine.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jul 2026 06:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45B41Z-EVK-not-programming-over-on-board-Debugger-MCU-Link/m-p/2399821#M68452</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2026-07-29T06:40:27Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z EVK not programming over on board Debugger MCU Link.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45B41Z-EVK-not-programming-over-on-board-Debugger-MCU-Link/m-p/2415672#M68519</link>
      <description>&lt;P&gt;Since the Secure Provisioning Tool can successfully flash and run code on the chip, the physical hardware is completely fine, meaning the "0 SWD Devices detected" error stems from a communication mismatch between your IDE's debug probe server and the onboard MCU-Link firmware. This is usually resolved by updating the MCU-Link firmware to the latest version compatible with your IDE, or by manually holding down the reset button during the connection sequence to prevent a low-power application state from locking out the debug interface.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Sep 2026 10:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45B41Z-EVK-not-programming-over-on-board-Debugger-MCU-Link/m-p/2415672#M68519</guid>
      <dc:creator>craig15miller</dc:creator>
      <dc:date>2026-09-23T10:00:01Z</dc:date>
    </item>
  </channel>
</rss>