<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: S9KEAZN8 – Low power mode entry code example and PWM signal detection in sleep</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8-Low-power-mode-entry-code-example-and-PWM-signal/m-p/2413865#M68510</link>
    <description>&lt;P&gt;For the S9KEAZN8, set low-power mode by setting the required clock/power configurations, and execute the appropriate WFI (Wait For Interrupt) instruction; the exact mode and wake-up sources depend on the S9KEAZN8 power-management module. For PWM monitoring, normally the MCU cannot measure PWM changes continuously when deeply asleep, so set-up an interrupt capable timer/input-capture channel or an external interrupt as the wake-up source; when an edge is detected, wake-up the MCU and use the timer/input-capture peripheral to measure the PWM period/duty cycle. Make sure to check the low-power wake-up/clock limitations of your device carefully as some peripherals and clocks are disabled in the deeper low-power modes.&lt;/P&gt;</description>
    <pubDate>Wed, 16 Sep 2026 05:22:35 GMT</pubDate>
    <dc:creator>david85burger</dc:creator>
    <dc:date>2026-09-16T05:22:35Z</dc:date>
    <item>
      <title>S9KEAZN8 – Low power mode entry code example and PWM signal detection in sleep</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8-Low-power-mode-entry-code-example-and-PWM-signal/m-p/2375515#M68389</link>
      <description>&lt;P class=""&gt;&lt;SPAN class=""&gt;I am using S9KEAZN8. I would like to know how to enter low power mode. Could anyone provide a code example showing how to do this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Also, I need to detect PWM signal changes while the MCU is in low power mode. What would be the proper way to handle this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;The Reference Manual does not have code examples. Any sample code or guidance would be appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jun 2026 05:42:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8-Low-power-mode-entry-code-example-and-PWM-signal/m-p/2375515#M68389</guid>
      <dc:creator>ssjj</dc:creator>
      <dc:date>2026-06-03T05:42:52Z</dc:date>
    </item>
    <item>
      <title>Re: S9KEAZN8 – Low power mode entry code example and PWM signal detection in sleep</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8-Low-power-mode-entry-code-example-and-PWM-signal/m-p/2375655#M68393</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263398"&gt;@ssjj&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;Which IDE are you using? If you are using S32DS, there are example projects available for KEA128. These examples can also be used for KEA8 with minor modifications.&lt;/P&gt;
&lt;DIV&gt;About enter low power mode, you can enter through the WFI instruction. For the specific implementation, you can refer to the pmc.c file, which includes functions such as PMC_SetMode().&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;If you have any other questions, please feel free to get back to me.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Wed, 03 Jun 2026 09:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8-Low-power-mode-entry-code-example-and-PWM-signal/m-p/2375655#M68393</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-06-03T09:18:40Z</dc:date>
    </item>
    <item>
      <title>Re: S9KEAZN8 – Low power mode entry code example and PWM signal detection in sleep</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8-Low-power-mode-entry-code-example-and-PWM-signal/m-p/2413865#M68510</link>
      <description>&lt;P&gt;For the S9KEAZN8, set low-power mode by setting the required clock/power configurations, and execute the appropriate WFI (Wait For Interrupt) instruction; the exact mode and wake-up sources depend on the S9KEAZN8 power-management module. For PWM monitoring, normally the MCU cannot measure PWM changes continuously when deeply asleep, so set-up an interrupt capable timer/input-capture channel or an external interrupt as the wake-up source; when an edge is detected, wake-up the MCU and use the timer/input-capture peripheral to measure the PWM period/duty cycle. Make sure to check the low-power wake-up/clock limitations of your device carefully as some peripherals and clocks are disabled in the deeper low-power modes.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Sep 2026 05:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8-Low-power-mode-entry-code-example-and-PWM-signal/m-p/2413865#M68510</guid>
      <dc:creator>david85burger</dc:creator>
      <dc:date>2026-09-16T05:22:35Z</dc:date>
    </item>
  </channel>
</rss>