<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックSDK 2.6.6 configuration error on MKE02 using MCUXpresso ide</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SDK-2-6-6-configuration-error-on-MKE02-using-MCUXpresso-ide/m-p/2409259#M68494</link>
    <description>&lt;PRE&gt;&lt;SPAN class=""&gt;After downloading the file SDK_26_06_00_MKE02Z64xxx4.zip and attempting to install it in MCUXpresso IDE, the following error occurs:
"MCUXpresso IDE was unable to load one or more SDK(s)". The same procedure used for the MKE02 and MKE15 did not produce any errors. Looking in the "doc" directory on SDK_26_06_00_MKE02Z64xxx4.zip, it appears that the file is relates to the MCUXpresso SDK rather than the MCUXpresso IDE, even though it was downloaded for the latter. How can this error be resolved? Where can I find the same file, but for MCUXpresso IDE?  Best regards, Carlo&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 28 Aug 2026 13:52:46 GMT</pubDate>
    <dc:creator>CarloC</dc:creator>
    <dc:date>2026-08-28T13:52:46Z</dc:date>
    <item>
      <title>SDK 2.6.6 configuration error on MKE02 using MCUXpresso ide</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SDK-2-6-6-configuration-error-on-MKE02-using-MCUXpresso-ide/m-p/2409259#M68494</link>
      <description>&lt;PRE&gt;&lt;SPAN class=""&gt;After downloading the file SDK_26_06_00_MKE02Z64xxx4.zip and attempting to install it in MCUXpresso IDE, the following error occurs:
"MCUXpresso IDE was unable to load one or more SDK(s)". The same procedure used for the MKE02 and MKE15 did not produce any errors. Looking in the "doc" directory on SDK_26_06_00_MKE02Z64xxx4.zip, it appears that the file is relates to the MCUXpresso SDK rather than the MCUXpresso IDE, even though it was downloaded for the latter. How can this error be resolved? Where can I find the same file, but for MCUXpresso IDE?  Best regards, Carlo&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Aug 2026 13:52:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SDK-2-6-6-configuration-error-on-MKE02-using-MCUXpresso-ide/m-p/2409259#M68494</guid>
      <dc:creator>CarloC</dc:creator>
      <dc:date>2026-08-28T13:52:46Z</dc:date>
    </item>
    <item>
      <title>Re: SDK 2.6.6 configuration error on MKE02 using MCUXpresso ide</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SDK-2-6-6-configuration-error-on-MKE02-using-MCUXpresso-ide/m-p/2409315#M68495</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Could you help us confirm which MCUXpresso IDE are you using?&lt;/P&gt;
&lt;P&gt;It could be the version of IDE that are you using is old in comparation to the SDK version. I try using the MCUXpresso version v25.6 and it works.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you help us confirm if the toolchain selected in &lt;A href="https://mcuxpresso.nxp.com/dashboard" target="_blank"&gt;SDK builder&lt;/A&gt; when creating the SDK is MCUXpresso IDE?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="luis_maravilla_1-1787959664853.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395514i15638C348093F088/image-size/medium?v=v2&amp;amp;px=400" role="button" title="luis_maravilla_1-1787959664853.png" alt="luis_maravilla_1-1787959664853.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;luis_maravilla_1-1787959664853.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If it was a different toolchain, this also could be the root cause.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you consider using &lt;A href="https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-for-visual-studio-code:MCUXPRESSO-VSC" target="_blank"&gt;MCUXpresso for Visual Studio Code&lt;/A&gt;? The SDK_26_06_00_MKE02Z64xxx4 is also available in that platform; let me know if you want to use this option and if you need more information.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
      <pubDate>Fri, 28 Aug 2026 23:28:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SDK-2-6-6-configuration-error-on-MKE02-using-MCUXpresso-ide/m-p/2409315#M68495</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-08-28T23:28:32Z</dc:date>
    </item>
  </channel>
</rss>