<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKE18F512VLH16 ECC Memory Cell Autocorrection</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-Memory-Cell-Autocorrection/m-p/2402601#M68459</link>
    <description>&lt;P&gt;It's understood that the HW provides automatic correction of single bit ECC errors. However, it's unclear where the corrections are being made.&lt;/P&gt;&lt;P&gt;When the hardware autocorrects a single bit ECC error, does it correct on both the read out and the memory cell, or just on the read out?&lt;/P&gt;&lt;P&gt;From the AN5335 example figure, is the Read-out Data being corrected from 0-&amp;gt;1? That would mean we need to write back the corrected value to RAM to actually clear it within the memory cell.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sean_dvorscak_0-1786035276314.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393899i971C6CDB0F7D7D81/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sean_dvorscak_0-1786035276314.png" alt="sean_dvorscak_0-1786035276314.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are concerned if the data in the RAM memory cell is not corrected, a single bit error could degrade to a double bit error.&lt;/P&gt;</description>
    <pubDate>Thu, 06 Aug 2026 17:03:26 GMT</pubDate>
    <dc:creator>sean_dvorscak</dc:creator>
    <dc:date>2026-08-06T17:03:26Z</dc:date>
    <item>
      <title>KE18F512VLH16 ECC Memory Cell Autocorrection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-Memory-Cell-Autocorrection/m-p/2402601#M68459</link>
      <description>&lt;P&gt;It's understood that the HW provides automatic correction of single bit ECC errors. However, it's unclear where the corrections are being made.&lt;/P&gt;&lt;P&gt;When the hardware autocorrects a single bit ECC error, does it correct on both the read out and the memory cell, or just on the read out?&lt;/P&gt;&lt;P&gt;From the AN5335 example figure, is the Read-out Data being corrected from 0-&amp;gt;1? That would mean we need to write back the corrected value to RAM to actually clear it within the memory cell.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sean_dvorscak_0-1786035276314.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393899i971C6CDB0F7D7D81/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sean_dvorscak_0-1786035276314.png" alt="sean_dvorscak_0-1786035276314.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are concerned if the data in the RAM memory cell is not corrected, a single bit error could degrade to a double bit error.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Aug 2026 17:03:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-Memory-Cell-Autocorrection/m-p/2402601#M68459</guid>
      <dc:creator>sean_dvorscak</dc:creator>
      <dc:date>2026-08-06T17:03:26Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F512VLH16 ECC Memory Cell Autocorrection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-Memory-Cell-Autocorrection/m-p/2402778#M68460</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/90401"&gt;@sean_dvorscak&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. "&lt;SPAN&gt;When the hardware autocorrects a single bit ECC error, does it correct on both the read out and the memory cell, or just on the read out?&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt;The correction is performed only on readout; the SRAM cell contents are not written back.&lt;/P&gt;
&lt;P&gt;2. "&lt;SPAN&gt;We are concerned if the data in the RAM memory cell is not corrected, a single bit error could degrade to a double bit error.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt;Yes, if you want to clear errors in the memory cells and prevent error accumulation, it is recommended that the software perform a read-correct-writeback operation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 07 Aug 2026 08:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F512VLH16-ECC-Memory-Cell-Autocorrection/m-p/2402778#M68460</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-08-07T08:11:02Z</dc:date>
    </item>
  </channel>
</rss>