<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DTM software to work with R&amp;amp;S CMW500 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/DTM-software-to-work-with-R-amp-S-CMW500/m-p/2380381#M68405</link>
    <description>&lt;P lang="es-419"&gt;Hello, hope you are doing well!&lt;/P&gt;
&lt;P lang="es-419"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P lang="es-419"&gt;&lt;SPAN&gt;This application note provides the RF evaluation test result of the KW45B41Z-EVK for BLE applications using the connectivity_test and HCI_bb application examples&lt;/SPAN&gt;: &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13228" target="_blank"&gt;AN13228 KW45B41Z-EVK RF System Evaluation Report for Bluetooth Low Energy Applications&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, maybe these posts could be helpful:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Wireless-MCU/How-to-use-the-HCI-bb-on-Kinetis-family-products-and-get-access/m-p/1272092#M11118" target="_blank"&gt;How to use the HCI_bb on Kinetis family products and get access to the DTM mode&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;This article is presenting two parts:&lt;BR /&gt;How to flash the HCI_bb binary into the Kinetis product.&lt;BR /&gt;Perform RF measurement using the R&amp;amp;S CMW270&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/BLE-HCI-Application-to-set-transmitter-receiver-test-commands/ta-p/1126093" target="_blank"&gt;BLE HCI Application to set transmitter/receiver test commands&lt;/A&gt;&lt;BR /&gt;This article provides the steps to show how user could send serial commands to the device.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/Bluetooth-LE-HCI-Black-Box-Quick-Start-Guide/ta-p/1099874" target="_blank"&gt;Bluetooth LE HCI Black Box Quick Start Guide&lt;/A&gt;&lt;BR /&gt;This article describes a simple process for enabling the user controls the radio through serial commands.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P lang="es-419"&gt;Best regards,&lt;BR /&gt;Sofia.&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jun 2026 19:53:27 GMT</pubDate>
    <dc:creator>sofiaurueta</dc:creator>
    <dc:date>2026-06-11T19:53:27Z</dc:date>
    <item>
      <title>DTM software to work with R&amp;S CMW500</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/DTM-software-to-work-with-R-amp-S-CMW500/m-p/2379290#M68404</link>
      <description>&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to work on KW45B41Z-EVK board with R&amp;amp;S CMW500 equipment for BLE testing directly but I found the following problem on it.&lt;/P&gt;&lt;P&gt;1) R&amp;amp;S CMW500 can recognize the USB visual COM driver for the kit but I cannot find the driver file for the MCU-Link and my equipment seems to be windows based system so I need how to download windows driver for the kit.&lt;/P&gt;&lt;P&gt;2) For the software running in EVK, I load the example code of hci_bb_bm code on it and it can run Generic FSK connectivity test demo software thru TeraTerm and try to connect this COM port into CMW500 and the initial check on the DTM connection with equipment is passed but EVK board seems to be not able to response to read test command from equipment and then making any BLE RF PHY link testing.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Therefore, I don't sure any specific software from NXP to be fit with DTM interface with equipment directly or any advise for using hci_bb_bm software to run with DTM with standard BLE tester equipment included R&amp;amp;S CMW500.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jun 2026 05:39:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/DTM-software-to-work-with-R-amp-S-CMW500/m-p/2379290#M68404</guid>
      <dc:creator>hungli33</dc:creator>
      <dc:date>2026-06-10T05:39:36Z</dc:date>
    </item>
    <item>
      <title>Re: DTM software to work with R&amp;S CMW500</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/DTM-software-to-work-with-R-amp-S-CMW500/m-p/2380381#M68405</link>
      <description>&lt;P lang="es-419"&gt;Hello, hope you are doing well!&lt;/P&gt;
&lt;P lang="es-419"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P lang="es-419"&gt;&lt;SPAN&gt;This application note provides the RF evaluation test result of the KW45B41Z-EVK for BLE applications using the connectivity_test and HCI_bb application examples&lt;/SPAN&gt;: &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13228" target="_blank"&gt;AN13228 KW45B41Z-EVK RF System Evaluation Report for Bluetooth Low Energy Applications&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, maybe these posts could be helpful:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Wireless-MCU/How-to-use-the-HCI-bb-on-Kinetis-family-products-and-get-access/m-p/1272092#M11118" target="_blank"&gt;How to use the HCI_bb on Kinetis family products and get access to the DTM mode&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;This article is presenting two parts:&lt;BR /&gt;How to flash the HCI_bb binary into the Kinetis product.&lt;BR /&gt;Perform RF measurement using the R&amp;amp;S CMW270&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/BLE-HCI-Application-to-set-transmitter-receiver-test-commands/ta-p/1126093" target="_blank"&gt;BLE HCI Application to set transmitter/receiver test commands&lt;/A&gt;&lt;BR /&gt;This article provides the steps to show how user could send serial commands to the device.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/Bluetooth-LE-HCI-Black-Box-Quick-Start-Guide/ta-p/1099874" target="_blank"&gt;Bluetooth LE HCI Black Box Quick Start Guide&lt;/A&gt;&lt;BR /&gt;This article describes a simple process for enabling the user controls the radio through serial commands.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P lang="es-419"&gt;Best regards,&lt;BR /&gt;Sofia.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jun 2026 19:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/DTM-software-to-work-with-R-amp-S-CMW500/m-p/2380381#M68405</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2026-06-11T19:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: DTM software to work with R&amp;S CMW500</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/DTM-software-to-work-with-R-amp-S-CMW500/m-p/2408745#M68491</link>
      <description>&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;You’ll need the MCU‑Link Windows driver from NXP’s site (it’s bundled with MCUXpresso IDE/Drivers package), as the CMW500 only recognizes standard COM ports. For BLE DTM testing, the hci_bb_bm demo isn’t fully compliant with the DTM spec—NXP provides dedicated DTM firmware examples for KW45 boards that respond correctly to tester commands. Flashing that DTM example instead of hci_bb_bm should allow proper RF PHY link testing with the CMW500.&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Thu, 27 Aug 2026 08:48:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/DTM-software-to-work-with-R-amp-S-CMW500/m-p/2408745#M68491</guid>
      <dc:creator>iva89ward</dc:creator>
      <dc:date>2026-08-27T08:48:40Z</dc:date>
    </item>
  </channel>
</rss>