<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Inquiry on Slave Latency Override Support in NXP KW47 SDK in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Inquiry-on-Slave-Latency-Override-Support-in-NXP-KW47-SDK/m-p/2361237#M68339</link>
    <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I would like to check whether the &lt;STRONG&gt;NXP KW47 SDK supports the Slave Latency Override feature&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Specifically, in a BLE connection where the device is operating in the &lt;STRONG&gt;peripheral role&lt;/STRONG&gt;, is there any supported mechanism to &lt;STRONG&gt;temporarily disable or override slave latency&lt;/STRONG&gt; so that the peripheral can listen to packets from the BLE central for every connection event?&lt;/P&gt;&lt;P&gt;During our investigation, we came across the following API:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/**
 * @brief  Set the initial value for the slave latency inactive event counter
 *         After transmitting or receiving data the slave listens for 'counter'
 *         consecutive events after the last event where data was seen
 *         on the air. This can improve reactivity when packets are queued for
 *         transmission on the slave or when packets are transmitted by the master
 *         with a time gap of less than 'count' events.
 *
 * &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197964"&gt;@Param&lt;/a&gt;  counter : [in] The number of events the slave latency will be skipped
 *                   after data is transmitted or received
 * @retval ble_stat_t: command status
 */
ble_stat_t ll_intf_le_set_sl_inactive_initial_event_counter(uint16_t counter);&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;P&gt;Could you please confirm:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Whether this API is intended to support slave latency override or a similar behavior?&lt;/LI&gt;&lt;LI&gt;If there are any &lt;STRONG&gt;additional APIs, configuration options, or recommended approaches&lt;/STRONG&gt; in the KW47 SDK to temporarily disable slave latency or force the peripheral to remain active?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Your guidance on this would be very helpful for our implementation.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;BR /&gt;Looking forward to your response.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Nidhin&lt;/P&gt;&lt;/DIV&gt;</description>
    <pubDate>Wed, 06 May 2026 13:49:13 GMT</pubDate>
    <dc:creator>nidhintomy</dc:creator>
    <dc:date>2026-05-06T13:49:13Z</dc:date>
    <item>
      <title>Inquiry on Slave Latency Override Support in NXP KW47 SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Inquiry-on-Slave-Latency-Override-Support-in-NXP-KW47-SDK/m-p/2361237#M68339</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I would like to check whether the &lt;STRONG&gt;NXP KW47 SDK supports the Slave Latency Override feature&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Specifically, in a BLE connection where the device is operating in the &lt;STRONG&gt;peripheral role&lt;/STRONG&gt;, is there any supported mechanism to &lt;STRONG&gt;temporarily disable or override slave latency&lt;/STRONG&gt; so that the peripheral can listen to packets from the BLE central for every connection event?&lt;/P&gt;&lt;P&gt;During our investigation, we came across the following API:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/**
 * @brief  Set the initial value for the slave latency inactive event counter
 *         After transmitting or receiving data the slave listens for 'counter'
 *         consecutive events after the last event where data was seen
 *         on the air. This can improve reactivity when packets are queued for
 *         transmission on the slave or when packets are transmitted by the master
 *         with a time gap of less than 'count' events.
 *
 * &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197964"&gt;@Param&lt;/a&gt;  counter : [in] The number of events the slave latency will be skipped
 *                   after data is transmitted or received
 * @retval ble_stat_t: command status
 */
ble_stat_t ll_intf_le_set_sl_inactive_initial_event_counter(uint16_t counter);&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;P&gt;Could you please confirm:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Whether this API is intended to support slave latency override or a similar behavior?&lt;/LI&gt;&lt;LI&gt;If there are any &lt;STRONG&gt;additional APIs, configuration options, or recommended approaches&lt;/STRONG&gt; in the KW47 SDK to temporarily disable slave latency or force the peripheral to remain active?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Your guidance on this would be very helpful for our implementation.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;BR /&gt;Looking forward to your response.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Nidhin&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 06 May 2026 13:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Inquiry-on-Slave-Latency-Override-Support-in-NXP-KW47-SDK/m-p/2361237#M68339</guid>
      <dc:creator>nidhintomy</dc:creator>
      <dc:date>2026-05-06T13:49:13Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiry on Slave Latency Override Support in NXP KW47 SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Inquiry-on-Slave-Latency-Override-Support-in-NXP-KW47-SDK/m-p/2362610#M68350</link>
      <description>&lt;P lang="es-419"&gt;Hello,&lt;BR /&gt;Hope you are doing well.&lt;/P&gt;
&lt;P lang="es-419"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please let me know which KW47 SDK version you are using? Are you working with a specific SDK example project?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The &lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/middleware/wireless/bluetooth/doc/Bluetooth%20Low%20Energy%20Host%20Stack%20API%20Reference%20Manual/groups.html#c.Gap_LeSetLocalPeripheralLatencyEnable" target="_blank"&gt;Gap_LeSetLocalPeripheralLatencyEnable&lt;/A&gt; function can be used to enable or disable local Peripheral latency for an active connection:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;bleResult_t Gap_LeSetLocalPeripheralLatencyEnable(deviceId_t deviceId, bool_t enable)&lt;/LI-CODE&gt;
&lt;P&gt;Parameters:&lt;BR /&gt;deviceId – [in] Handle identifying the connection.&lt;BR /&gt;enable – [in] FALSE to disable, TRUE to enable local Peripheral latency.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Sofia.&lt;/P&gt;</description>
      <pubDate>Sat, 09 May 2026 00:27:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Inquiry-on-Slave-Latency-Override-Support-in-NXP-KW47-SDK/m-p/2362610#M68350</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2026-05-09T00:27:25Z</dc:date>
    </item>
  </channel>
</rss>