<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックUSB MSD Bootloader in GCC (CW 10.3)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-Bootloader-in-GCC-CW-10-3/m-p/248573#M6831</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone had any luck porting the USB Mass Storage Device Bootloader to CW 10.3 using GCC?&amp;nbsp; I've been able to port the CW 10.2 project to 10.3 using the Freescale toolchain, and that works fine.&amp;nbsp; When I move to using GCC, I've been able to get the project to compile and run on custom K60 hardware, but I get a USB Device Not Recognized error during USB enumeration.&amp;nbsp; I'm thinking that maybe I messed up something in the linker file (the default linker file adds in the extra C++ portions that didn't appear in the original) or in the startup code (currently have the project setup to use EWL).&amp;nbsp; As I continue to bang my head against the wall with checking everything, I was wondering if anyone has done this already or if someone had tips for other places to look for errors.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for your help,&lt;/P&gt;&lt;P&gt;-Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Feb 2013 23:48:48 GMT</pubDate>
    <dc:creator>michaelvernier</dc:creator>
    <dc:date>2013-02-05T23:48:48Z</dc:date>
    <item>
      <title>USB MSD Bootloader in GCC (CW 10.3)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-Bootloader-in-GCC-CW-10-3/m-p/248573#M6831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone had any luck porting the USB Mass Storage Device Bootloader to CW 10.3 using GCC?&amp;nbsp; I've been able to port the CW 10.2 project to 10.3 using the Freescale toolchain, and that works fine.&amp;nbsp; When I move to using GCC, I've been able to get the project to compile and run on custom K60 hardware, but I get a USB Device Not Recognized error during USB enumeration.&amp;nbsp; I'm thinking that maybe I messed up something in the linker file (the default linker file adds in the extra C++ portions that didn't appear in the original) or in the startup code (currently have the project setup to use EWL).&amp;nbsp; As I continue to bang my head against the wall with checking everything, I was wondering if anyone has done this already or if someone had tips for other places to look for errors.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for your help,&lt;/P&gt;&lt;P&gt;-Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2013 23:48:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-Bootloader-in-GCC-CW-10-3/m-p/248573#M6831</guid>
      <dc:creator>michaelvernier</dc:creator>
      <dc:date>2013-02-05T23:48:48Z</dc:date>
    </item>
    <item>
      <title>Re: USB MSD Bootloader in GCC (CW 10.3)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-Bootloader-in-GCC-CW-10-3/m-p/248574#M6832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think I have the same problem. I'm trying to port USB HID Device project to CrossWorks for ARM (GCC) and I alway get "Device not recongnized" in Windows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you had any luck with this issue? Or does anyone manage to run Freescale USB stack project using GCC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2013 08:18:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-Bootloader-in-GCC-CW-10-3/m-p/248574#M6832</guid>
      <dc:creator>gaminn</dc:creator>
      <dc:date>2013-03-14T08:18:38Z</dc:date>
    </item>
  </channel>
</rss>