<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MK66 serie with eMMC in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-serie-with-eMMC/m-p/2346117#M68300</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using a MK66 MCU serie and I was wondering if there is the possibility to drive an eMMC with the SDHC driver from the MK66. I don't want to work with a SD card.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know this is not a native configuration but is there a way to do this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding the risks, is it worth it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 07 Apr 2026 08:45:57 GMT</pubDate>
    <dc:creator>LeroyGG</dc:creator>
    <dc:date>2026-04-07T08:45:57Z</dc:date>
    <item>
      <title>MK66 serie with eMMC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-serie-with-eMMC/m-p/2346117#M68300</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using a MK66 MCU serie and I was wondering if there is the possibility to drive an eMMC with the SDHC driver from the MK66. I don't want to work with a SD card.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know this is not a native configuration but is there a way to do this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding the risks, is it worth it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 07 Apr 2026 08:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-serie-with-eMMC/m-p/2346117#M68300</guid>
      <dc:creator>LeroyGG</dc:creator>
      <dc:date>2026-04-07T08:45:57Z</dc:date>
    </item>
    <item>
      <title>Re: MK66 serie with eMMC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-serie-with-eMMC/m-p/2346763#M68301</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261427"&gt;@LeroyGG&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;In short, it is technically possible to access an eMMC device using the SDHC peripheral of the MK66.&lt;/P&gt;
&lt;P&gt;The SDHC peripheral on the MK66 is based on an SD/MMC host controller. The eMMC is backward-compatible with the MMC protocol. You may refer to the&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=K66P144M180SF5RMV2" target="_self"&gt;Reference Manual&lt;/A&gt;&amp;nbsp; for more details.&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Wed, 08 Apr 2026 07:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-serie-with-eMMC/m-p/2346763#M68301</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-04-08T07:29:02Z</dc:date>
    </item>
  </channel>
</rss>