<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFRDM-K66F completely bricked after wrong firmware flash — OpenSDA USB port not powering on</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-completely-bricked-after-wrong-firmware-flash-OpenSDA/m-p/2339591#M68278</link>
    <description>&lt;P class=""&gt;Hi everyone,&lt;/P&gt;&lt;P class=""&gt;I'm hoping someone can help me recover my FRDM-K66F board. I accidentally flashed an incorrect binary file while in bootloader/maintenance mode on the OpenSDAv2.1 interface. Since then, the board is completely unresponsive via the OpenSDA USB port.&lt;/P&gt;&lt;P class=""&gt;&lt;STRONG&gt;What I'm seeing:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;OpenSDA USB port (J26): Power LED does NOT turn on. No USB enumeration at all — the computer does not detect anything.&lt;/LI&gt;&lt;LI&gt;K66F USB port (J22): Power LED turns ON and the board powers up normally.&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;&lt;STRONG&gt;What I've tried so far:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Holding SW1 while plugging into J26 to enter bootloader mode — no response.&lt;/LI&gt;&lt;LI&gt;Powering the board through J22 first, then connecting J26 while holding SW1 — OpenSDA still doesn't enumerate.&lt;/LI&gt;&lt;LI&gt;Tested with multiple confirmed data USB cables.&lt;/LI&gt;&lt;LI&gt;Tested on multiple computers (Windows and Linux). On Linux, dmesg -w shows absolutely no USB device detection from J26.&lt;/LI&gt;&lt;LI&gt;Held SW1 for 10+ seconds before and after plugging in — no change.&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;&lt;STRONG&gt;My observations:&lt;/STRONG&gt; It seems like the OpenSDA power path (P5V_SDA_PSW) might be damaged, or the K20 chip firmware is completely corrupted. The fact that J22 powers the board fine suggests the 3.3V regulator and K66F MCU are OK.&lt;/P&gt;&lt;P class=""&gt;&lt;STRONG&gt;What I don't have:&lt;/STRONG&gt; I don't currently have access to an external SWD debugger (J-Link, etc.) to reflash the K20 through the J9 header.&lt;/P&gt;&lt;P class=""&gt;Has anyone recovered from this situation without an external debugger? Are there any other tricks I'm missing? Any help would be greatly appreciated.&lt;/P&gt;&lt;P class=""&gt;Board: FRDM-K66F MCU: MK66FN2M0VMD18 OpenSDA: v2.1 (K20 based)&lt;/P&gt;&lt;P class=""&gt;Thanks in advance!&lt;/P&gt;</description>
    <pubDate>Wed, 25 Mar 2026 19:48:28 GMT</pubDate>
    <dc:creator>wolfroger33</dc:creator>
    <dc:date>2026-03-25T19:48:28Z</dc:date>
    <item>
      <title>FRDM-K66F completely bricked after wrong firmware flash — OpenSDA USB port not powering on</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-completely-bricked-after-wrong-firmware-flash-OpenSDA/m-p/2339591#M68278</link>
      <description>&lt;P class=""&gt;Hi everyone,&lt;/P&gt;&lt;P class=""&gt;I'm hoping someone can help me recover my FRDM-K66F board. I accidentally flashed an incorrect binary file while in bootloader/maintenance mode on the OpenSDAv2.1 interface. Since then, the board is completely unresponsive via the OpenSDA USB port.&lt;/P&gt;&lt;P class=""&gt;&lt;STRONG&gt;What I'm seeing:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;OpenSDA USB port (J26): Power LED does NOT turn on. No USB enumeration at all — the computer does not detect anything.&lt;/LI&gt;&lt;LI&gt;K66F USB port (J22): Power LED turns ON and the board powers up normally.&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;&lt;STRONG&gt;What I've tried so far:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Holding SW1 while plugging into J26 to enter bootloader mode — no response.&lt;/LI&gt;&lt;LI&gt;Powering the board through J22 first, then connecting J26 while holding SW1 — OpenSDA still doesn't enumerate.&lt;/LI&gt;&lt;LI&gt;Tested with multiple confirmed data USB cables.&lt;/LI&gt;&lt;LI&gt;Tested on multiple computers (Windows and Linux). On Linux, dmesg -w shows absolutely no USB device detection from J26.&lt;/LI&gt;&lt;LI&gt;Held SW1 for 10+ seconds before and after plugging in — no change.&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;&lt;STRONG&gt;My observations:&lt;/STRONG&gt; It seems like the OpenSDA power path (P5V_SDA_PSW) might be damaged, or the K20 chip firmware is completely corrupted. The fact that J22 powers the board fine suggests the 3.3V regulator and K66F MCU are OK.&lt;/P&gt;&lt;P class=""&gt;&lt;STRONG&gt;What I don't have:&lt;/STRONG&gt; I don't currently have access to an external SWD debugger (J-Link, etc.) to reflash the K20 through the J9 header.&lt;/P&gt;&lt;P class=""&gt;Has anyone recovered from this situation without an external debugger? Are there any other tricks I'm missing? Any help would be greatly appreciated.&lt;/P&gt;&lt;P class=""&gt;Board: FRDM-K66F MCU: MK66FN2M0VMD18 OpenSDA: v2.1 (K20 based)&lt;/P&gt;&lt;P class=""&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Wed, 25 Mar 2026 19:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-completely-bricked-after-wrong-firmware-flash-OpenSDA/m-p/2339591#M68278</guid>
      <dc:creator>wolfroger33</dc:creator>
      <dc:date>2026-03-25T19:48:28Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F completely bricked after wrong firmware flash — OpenSDA USB port not powering on</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-completely-bricked-after-wrong-firmware-flash-OpenSDA/m-p/2340921#M68285</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260988"&gt;@wolfroger33&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;Based on your description, I’m afraid you must need to use an external debugger to re-flash the OpenSDA bootloader on the K20.&lt;BR /&gt;Additionally, I’d like to clarify that you should connect to the K20 through the J10 header, not J9.&lt;/P&gt;
&lt;P&gt;OpenSDA bootloader can be found here:&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/sensor-toolbox/opensda-serial-and-debug-adapter:OPENSDA?tid=vanOpenSDA#FRDM-K66F" target="_blank"&gt;OpenSDA Serial and Debug Adapter | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Mar 2026 09:22:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-completely-bricked-after-wrong-firmware-flash-OpenSDA/m-p/2340921#M68285</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-03-27T09:22:18Z</dc:date>
    </item>
  </channel>
</rss>