<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KV5 DMA and UART in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5-DMA-and-UART/m-p/2291885#M68150</link>
    <description>&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I imported the example for using the UART and DMA. The original example has the UART0. It works. I changed for using other ports, now I try with UART4 and it does not. I can see the callback called for the and of TX but never for the end of RX. I don t get the point. I am sure the pins and the connections are ok. I am using the tower system for the KV5.&amp;nbsp;&lt;BR /&gt;I drop here the example with minor modifications for changing the UART.&lt;BR /&gt;&lt;BR /&gt;Every help is welcome..&lt;BR /&gt;&lt;BR /&gt;Thank You&lt;BR /&gt;&lt;BR /&gt;Pietro&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 12 Jan 2026 16:53:22 GMT</pubDate>
    <dc:creator>pietrodicastri</dc:creator>
    <dc:date>2026-01-12T16:53:22Z</dc:date>
    <item>
      <title>KV5 DMA and UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5-DMA-and-UART/m-p/2291885#M68150</link>
      <description>&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I imported the example for using the UART and DMA. The original example has the UART0. It works. I changed for using other ports, now I try with UART4 and it does not. I can see the callback called for the and of TX but never for the end of RX. I don t get the point. I am sure the pins and the connections are ok. I am using the tower system for the KV5.&amp;nbsp;&lt;BR /&gt;I drop here the example with minor modifications for changing the UART.&lt;BR /&gt;&lt;BR /&gt;Every help is welcome..&lt;BR /&gt;&lt;BR /&gt;Thank You&lt;BR /&gt;&lt;BR /&gt;Pietro&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jan 2026 16:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5-DMA-and-UART/m-p/2291885#M68150</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2026-01-12T16:53:22Z</dc:date>
    </item>
    <item>
      <title>Re: KV5 DMA and UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5-DMA-and-UART/m-p/2291886#M68151</link>
      <description>&lt;P&gt;The file is here.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jan 2026 16:56:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5-DMA-and-UART/m-p/2291886#M68151</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2026-01-12T16:56:03Z</dc:date>
    </item>
    <item>
      <title>Re: KV5 DMA and UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5-DMA-and-UART/m-p/2291980#M68152</link>
      <description>&lt;P&gt;Hello Pietro&lt;/P&gt;
&lt;P&gt;Could you help us confirm which UART-DMA example are you using and which SDK version is it from?&lt;/P&gt;
&lt;P&gt;Could you help us share your connections?&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jan 2026 21:01:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5-DMA-and-UART/m-p/2291980#M68152</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-01-12T21:01:02Z</dc:date>
    </item>
  </channel>
</rss>