<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SdCard inserted block K60 boot in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248409#M6809</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Exactly but when a SD card is inserted, the signal is pull down. So I need to disable this functionnality.&lt;/P&gt;&lt;P&gt;The SD card will be inserted after the first programming of the microcontroller.&lt;/P&gt;&lt;P&gt;After it's no possible to have an acces to the sd card. So the SD card need to be inserted all the time after the first programming sequence.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Dec 2013 16:27:23 GMT</pubDate>
    <dc:creator>guillaumetiffin</dc:creator>
    <dc:date>2013-12-09T16:27:23Z</dc:date>
    <item>
      <title>SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248403#M6803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with a custom card and the MK60FX512VLQ15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a SDCARD connector. It is mapped on the pin 1, 2, 3, 4, 7 and 8 (SD1, SD0, SDCLK, SDCMD, SD3 and SD2).&lt;/P&gt;&lt;P&gt;The Card Detect signal is mapped to PTA4 (pin 54).&lt;/P&gt;&lt;P&gt;When I put a SDCARD inside, everything is ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is when I let the SDCARD inserted.&lt;/P&gt;&lt;P&gt;In this case the program don't boot and if I try to program it with the JTAG mapped from PTA0 to PTA3, the K60 cannot be reach.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I doing wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I correct this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for you ranswer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Guillaume &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2013 13:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248403#M6803</guid>
      <dc:creator>guillaumetiffin</dc:creator>
      <dc:date>2013-12-06T13:45:58Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248404#M6804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guillaume,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make sure your SD connector is connected to grounds like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41668iD092E20CC7ADDC92/image-size/large?v=v2&amp;amp;px=999" title="SD.PNG.png" alt="SD.PNG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Would be useful if you can post your SD custom board to take a look at it. I'll keep looking for the problem.&lt;BR /&gt;Keep me informed,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hector Sanchez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 15:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248404#M6804</guid>
      <dc:creator>hectorsanchez</dc:creator>
      <dc:date>2013-12-09T15:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248405#M6805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hector,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't post the schematic right now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SD Card slot is well connected. I checked it before. And it works well. Hte problem is only at the startup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After some investigation, it seems to have some conflicts with the EZP_CS signal. My SD_CARD_DETECT signal is on the EZP_CS pin.&lt;/P&gt;&lt;P&gt;When the card is inserted in the slot, the SD_CARD_DETECT signal is pull_down. So I think that the EzPort operation is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I think that I need to disable the EzPort and after set this pin as an IO. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if I don't change this option in the boot sequence, it won't works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to write the FOPT register but without any succes. I didn't find the right way to do this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you think that it could be the source of my problem?&lt;/P&gt;&lt;P&gt;If you think so, can you tell me how to do this please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Guillaume&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 15:35:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248405#M6805</guid>
      <dc:creator>guillaumetiffin</dc:creator>
      <dc:date>2013-12-09T15:35:48Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248406#M6806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guillaume,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is , if the EZP_CS pin is low on reset, the k60 will enter EZP mode as stated here:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41732iC2EB6E90A5B468AB/image-size/large?v=v2&amp;amp;px=999" title="EZP_CS.png" alt="EZP_CS.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would try to set the Reset Signal pin to High and see if i can set the pin as an I/O, i don't have my board right now but i will try as soon as possible if this can be done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The EzProg can operate as a MicroSD card reader, i recommend you to read this AN: &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4406.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation"&gt;AN4406&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking for a workaround right now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keep me informed,&lt;/P&gt;&lt;P&gt;Hector Sanchez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 16:03:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248406#M6806</guid>
      <dc:creator>hectorsanchez</dc:creator>
      <dc:date>2013-12-09T16:03:13Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248407#M6807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hector,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your help. It's very nice to you to help me.&lt;/P&gt;&lt;P&gt;It's my first board with a Freescale's product. So I'm facing some problems wich can be really silly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The EZP port mode problem, is exactly what I thought but I didn't find the way to write to the register to disable this option. I just have to write a 0 instead of a 1 (0xFD)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41810i40991EF64B942576/image-size/large?v=v2&amp;amp;px=999" title="EZP_CS.png" alt="EZP_CS.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you know the way to do, please tell me and I'll try it. &lt;/P&gt;&lt;P&gt;I think that it's possible to use it as a GPIO because I already use it as a GPIO but the pin is not pull down during startup.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Guillaume&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 16:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248407#M6807</guid>
      <dc:creator>guillaumetiffin</dc:creator>
      <dc:date>2013-12-09T16:18:48Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248408#M6808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: if &lt;SPAN style="font-size: 12.0pt; font-family: 'Calibri','sans-serif';"&gt;EZP_CS rises with VDD the board will not enter EZPort.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 16:20:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248408#M6808</guid>
      <dc:creator>hectorsanchez</dc:creator>
      <dc:date>2013-12-09T16:20:17Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248409#M6809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Exactly but when a SD card is inserted, the signal is pull down. So I need to disable this functionnality.&lt;/P&gt;&lt;P&gt;The SD card will be inserted after the first programming of the microcontroller.&lt;/P&gt;&lt;P&gt;After it's no possible to have an acces to the sd card. So the SD card need to be inserted all the time after the first programming sequence.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 16:27:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248409#M6809</guid>
      <dc:creator>guillaumetiffin</dc:creator>
      <dc:date>2013-12-09T16:27:23Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248410#M6810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi , I'm glad to help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to do it the software way, put this in your code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FTFE_FOPT &amp;amp;= ~(0x02);&amp;nbsp; // EZPORT_DIS cleared , EZPort Operation disabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// This is just to make sure it disables the EZport mode pins&lt;/P&gt;&lt;P&gt;PORTA_PCR6 |= PORT_PCR_MUX(1)&amp;nbsp; // Set PortA pin 6 as PTA6 function&lt;/P&gt;&lt;P&gt;PORTA_PCR4 |= PORT_PCR_MUX(0)&amp;nbsp; // Set PortA pin 4 as IO (EZP_CS_b)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 16:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248410#M6810</guid>
      <dc:creator>hectorsanchez</dc:creator>
      <dc:date>2013-12-09T16:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248411#M6811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried your solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It doesn't work. Here is the test code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; printf("\n FTFE_FOPT = %d \n", FTFE_FOPT);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; printf("\n NV_FOPT = %d \n", NV_FOPT);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; FTFE_FOPT &amp;amp;= ~(0x02);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; printf("\n FTFE_FOPT = %d \n", FTFE_FOPT);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; printf("\n NV_FOPT = %d \n", NV_FOPT);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After a restart I still have the same value (255 instead of 253).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried&lt;/P&gt;&lt;P&gt;#define SET_FOPT @0x040D = 0xFD;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But with the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried&lt;/P&gt;&lt;P&gt;NV_FOPT = 0xFD;&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;FTFE_FlashConfig_BASE_PTR-&amp;gt;FOPT = 0xFD;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but the program stop.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 17:01:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248411#M6811</guid>
      <dc:creator>guillaumetiffin</dc:creator>
      <dc:date>2013-12-09T17:01:50Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248412#M6812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same problem currently.&lt;/P&gt;&lt;P&gt;Due to the wiring of the EZP_CS - pin of my K60 (I want to use this pin as PWM output) I need to disable the EZP functionality.&lt;/P&gt;&lt;P&gt;Can anyone tell me how to do this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Georg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 11:44:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248412#M6812</guid>
      <dc:creator>georgschmidt</dc:creator>
      <dc:date>2014-04-28T11:44:51Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248413#M6813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got the same problem, here is my solution:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You must set NV_OPT, because FTFL_OPT is loaded with the value NV_FOPT at each reset. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But you cannot just dynamically set NV_FOPT = 0xFD, because NV_FOPT resides in the program flash sector.&lt;/P&gt;&lt;P&gt;So you have to find the the sector cfmconfig in your code,change it, and recompile .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that if you use mqx(4.1.1), PEx will not do the expected job because the bsp values take the place in this sector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After checking that the register FTFL_OPT is now correct, if you still have problems, look a the NMI ...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 15:11:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248413#M6813</guid>
      <dc:creator>lvw</dc:creator>
      <dc:date>2014-09-09T15:11:08Z</dc:date>
    </item>
    <item>
      <title>Re: SdCard inserted block K60 boot</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248414#M6814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Georg Schmidt:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you resolve your doubt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EZPORT can be disabled from the NV_FOPT flash space. The next thread provides some hints about this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/452496"&gt;Re: How to modify FTFL_FOPT register on Kinetis K10 to change boot options?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Feb 2015 00:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SdCard-inserted-block-K60-boot/m-p/248414#M6814</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-02-07T00:20:08Z</dc:date>
    </item>
  </channel>
</rss>