<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックTime Sync between central device and multiple peripheral devices.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Time-Sync-between-central-device-and-multiple-peripheral-devices/m-p/2182690#M67938</link>
    <description>&lt;P&gt;Hello NXP team,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using Kw45 evk board as peripheral and Kw45-LOC as central.&lt;/P&gt;&lt;P&gt;I am sending time sync to multiple devices using single Central devices, but it seems that time is not synced properly and there is a gap of 1-2 seconds between the time of sensors.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using LPTMR to store milliseconds&lt;/P&gt;</description>
    <pubDate>Thu, 09 Oct 2025 05:07:58 GMT</pubDate>
    <dc:creator>ParikS</dc:creator>
    <dc:date>2025-10-09T05:07:58Z</dc:date>
    <item>
      <title>Time Sync between central device and multiple peripheral devices.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Time-Sync-between-central-device-and-multiple-peripheral-devices/m-p/2182690#M67938</link>
      <description>&lt;P&gt;Hello NXP team,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using Kw45 evk board as peripheral and Kw45-LOC as central.&lt;/P&gt;&lt;P&gt;I am sending time sync to multiple devices using single Central devices, but it seems that time is not synced properly and there is a gap of 1-2 seconds between the time of sensors.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using LPTMR to store milliseconds&lt;/P&gt;</description>
      <pubDate>Thu, 09 Oct 2025 05:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Time-Sync-between-central-device-and-multiple-peripheral-devices/m-p/2182690#M67938</guid>
      <dc:creator>ParikS</dc:creator>
      <dc:date>2025-10-09T05:07:58Z</dc:date>
    </item>
    <item>
      <title>Re: Time Sync between central device and multiple peripheral devices.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Time-Sync-between-central-device-and-multiple-peripheral-devices/m-p/2184039#M67947</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To better understand the situation, could you share more information about your application?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What SDK version are you using? Are you using an SDK example as base? And how are you configuring and enabling LPTMR in your application?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Ana Sofia.&lt;/P&gt;</description>
      <pubDate>Fri, 10 Oct 2025 18:41:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Time-Sync-between-central-device-and-multiple-peripheral-devices/m-p/2184039#M67947</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2025-10-10T18:41:41Z</dc:date>
    </item>
  </channel>
</rss>