<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Trigger ADC1 and ADC2 simultaneously with Software in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Trigger-ADC1-and-ADC2-simultaneously-with-Software/m-p/2179318#M67928</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;MKE18F512VLL16 microcontroller. I have configured ADC1 and ADC2 modules to sample different pins. Right now, I trigger the conversion 1 by 1. i.e. Start ADC1 conversion by writing SC1 of ADC1 and next writing SC1 of ADC2 and wait till both the conversions are completed. But the problem here is I am triggering ADCs one by one. &lt;STRONG&gt;I need to trigger both ADC conversion simultaneously and that trigger should be a software. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I attempted to use TRGMUX peripheral like below&lt;/P&gt;&lt;P&gt;1. Select SIM_SW_TRIG as input source for TRGMUX1 and output that Signal to TRGMUX0.&lt;/P&gt;&lt;P&gt;2. I selected EXTRG0, ADC1 and ADC2 module's trigger source as TRGMUX0's output.&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. I routed the EXTRG0 output to pin PTE16 and that pin is working as per the expectation when I write to SIM-&amp;gt;&lt;SPAN&gt;MISCTRL register.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;But ADC1 and ADC2 are not triggered. I confirmed it by putting the breakpoint inside the Conversion complete interrupt and it is not hit.&lt;/P&gt;&lt;P&gt;I need inputs on how I can achieve the requirement of simultaneous sampling. Please support ASAP as this is a time critical project for the company&lt;/P&gt;</description>
    <pubDate>Thu, 02 Oct 2025 12:03:26 GMT</pubDate>
    <dc:creator>Ruthrapathy_K</dc:creator>
    <dc:date>2025-10-02T12:03:26Z</dc:date>
    <item>
      <title>Trigger ADC1 and ADC2 simultaneously with Software</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Trigger-ADC1-and-ADC2-simultaneously-with-Software/m-p/2179318#M67928</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;MKE18F512VLL16 microcontroller. I have configured ADC1 and ADC2 modules to sample different pins. Right now, I trigger the conversion 1 by 1. i.e. Start ADC1 conversion by writing SC1 of ADC1 and next writing SC1 of ADC2 and wait till both the conversions are completed. But the problem here is I am triggering ADCs one by one. &lt;STRONG&gt;I need to trigger both ADC conversion simultaneously and that trigger should be a software. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I attempted to use TRGMUX peripheral like below&lt;/P&gt;&lt;P&gt;1. Select SIM_SW_TRIG as input source for TRGMUX1 and output that Signal to TRGMUX0.&lt;/P&gt;&lt;P&gt;2. I selected EXTRG0, ADC1 and ADC2 module's trigger source as TRGMUX0's output.&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. I routed the EXTRG0 output to pin PTE16 and that pin is working as per the expectation when I write to SIM-&amp;gt;&lt;SPAN&gt;MISCTRL register.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;But ADC1 and ADC2 are not triggered. I confirmed it by putting the breakpoint inside the Conversion complete interrupt and it is not hit.&lt;/P&gt;&lt;P&gt;I need inputs on how I can achieve the requirement of simultaneous sampling. Please support ASAP as this is a time critical project for the company&lt;/P&gt;</description>
      <pubDate>Thu, 02 Oct 2025 12:03:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Trigger-ADC1-and-ADC2-simultaneously-with-Software/m-p/2179318#M67928</guid>
      <dc:creator>Ruthrapathy_K</dc:creator>
      <dc:date>2025-10-02T12:03:26Z</dc:date>
    </item>
    <item>
      <title>Re: Trigger ADC1 and ADC2 simultaneously with Software</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Trigger-ADC1-and-ADC2-simultaneously-with-Software/m-p/2180068#M67930</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255021"&gt;@Ruthrapathy_K&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;As mentioned on the following post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Teensy-3-6-ADC-Simultaneous-Data-Read-Process/m-p/840591" target="_blank"&gt;K66 Teensy 3.6 ADC Simultaneous Data Read Process - NXP Community&lt;/A&gt;, you can use PDB to trigger ADC0 with&amp;nbsp;&lt;SPAN&gt;PDB CH0, and ADC1 with&amp;nbsp;PDB CH1. The following training material explains the usage of PDB, its functionality, and how to set it up:&amp;nbsp;&lt;A href="https://www.nxp.com.cn/docs/en/supporting-information/Programmable-Delay-Block-Training.pdf" target="_blank"&gt;PDB for Kinetis K Series MCUs | Training - PDF&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR,&lt;BR /&gt;Edwin.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Oct 2025 19:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Trigger-ADC1-and-ADC2-simultaneously-with-Software/m-p/2180068#M67930</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-10-03T19:52:17Z</dc:date>
    </item>
  </channel>
</rss>