<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックUSBDM vs PEMicro Initializations</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-vs-PEMicro-Initializations/m-p/2166694#M67873</link>
    <description>&lt;P&gt;I have some software for a FRDM-KE06Z demonstration board which communicates over the CANBus.&amp;nbsp; It works when connected using USBDM, but it does not work when not connected to a debugger.&amp;nbsp; It also does not work when connected using PEMicro open debugger, though the software is running and the basic functionality is there--just no CanBus communication as far as I can see.&amp;nbsp; I have checked Canbus frequencies for individual components with a scope and all seems good.&lt;/P&gt;&lt;P&gt;Are there any known differences in initialization between the USBDM debugger and the PEMico debugger which might help me determine what is lacking?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to dump all the registers from the running software to a file, so I can compare differences between the two different debugging instances?&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;</description>
    <pubDate>Wed, 10 Sep 2025 13:00:16 GMT</pubDate>
    <dc:creator>andrewmeyerbti</dc:creator>
    <dc:date>2025-09-10T13:00:16Z</dc:date>
    <item>
      <title>USBDM vs PEMicro Initializations</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-vs-PEMicro-Initializations/m-p/2166694#M67873</link>
      <description>&lt;P&gt;I have some software for a FRDM-KE06Z demonstration board which communicates over the CANBus.&amp;nbsp; It works when connected using USBDM, but it does not work when not connected to a debugger.&amp;nbsp; It also does not work when connected using PEMicro open debugger, though the software is running and the basic functionality is there--just no CanBus communication as far as I can see.&amp;nbsp; I have checked Canbus frequencies for individual components with a scope and all seems good.&lt;/P&gt;&lt;P&gt;Are there any known differences in initialization between the USBDM debugger and the PEMico debugger which might help me determine what is lacking?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to dump all the registers from the running software to a file, so I can compare differences between the two different debugging instances?&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;</description>
      <pubDate>Wed, 10 Sep 2025 13:00:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-vs-PEMicro-Initializations/m-p/2166694#M67873</guid>
      <dc:creator>andrewmeyerbti</dc:creator>
      <dc:date>2025-09-10T13:00:16Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM vs PEMicro Initializations</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-vs-PEMicro-Initializations/m-p/2167983#M67877</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/40522"&gt;@andrewmeyerbti&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you help me with the following questions?&lt;/P&gt;
&lt;P&gt;Which IDE are you using?&lt;BR /&gt;Are you using an SDK?&lt;BR /&gt;Have you made any changes to the project configuration?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Thu, 11 Sep 2025 16:46:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-vs-PEMicro-Initializations/m-p/2167983#M67877</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-09-11T16:46:23Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM vs PEMicro Initializations</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-vs-PEMicro-Initializations/m-p/2168923#M67881</link>
      <description>&lt;P&gt;Hi Pablo,&lt;/P&gt;&lt;P&gt;I'm using Kinetis Design Studio V3.2.0 which I believe uses a kinetics SDK which it installs itself, so not quite sure what version.&amp;nbsp; I didn't make any intentional changes to the project configurations--that being said sometimes mysterious things happen even on my isolated network.&lt;/P&gt;&lt;P&gt;Andy&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Sep 2025 12:02:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-vs-PEMicro-Initializations/m-p/2168923#M67881</guid>
      <dc:creator>andrewmeyerbti</dc:creator>
      <dc:date>2025-09-12T12:02:09Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM vs PEMicro Initializations</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-vs-PEMicro-Initializations/m-p/2188529#M67975</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I apologize for the inconvenience, but we do not have any guide or information to share on the related topic.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Pablo&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Oct 2025 21:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USBDM-vs-PEMicro-Initializations/m-p/2188529#M67975</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-10-17T21:51:31Z</dc:date>
    </item>
  </channel>
</rss>