<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックBuild Error with KM256SW3PHMET_R4_0_0: Fatal Error[Lp049] Related to __iar_data_init3</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-Error-with-KM256SW3PHMET-R4-0-0-Fatal-Error-Lp049-Related/m-p/2095821#M67538</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;I downloaded and installed the Three-Phase Power Meter Reference Design Software from the following NXP link:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/three-phase-power-meter-reference-design:THREE-PHASE-POWER-METER" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/three-phase-power-meter-reference-design:THREE-PHASE-POWER-METER&lt;/A&gt;&lt;/P&gt;&lt;P&gt;After installation, I tried to build the project located at:&lt;BR /&gt;C:\freescale\KM256SW3PHMET_R4_0_0\build\iar_7_40\projects\KM256SW3PHMET_R4_0_0&lt;BR /&gt;using IAR Embedded Workbench.&lt;/P&gt;&lt;P&gt;However, I encountered the following error during compilation:&lt;/P&gt;&lt;P&gt;Fatal Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss (adc.o #8)&lt;BR /&gt;I haven't modified any part of the project after installation. Could you please help me understand why this error occurs and how to resolve it?&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Tue, 13 May 2025 01:24:40 GMT</pubDate>
    <dc:creator>MSCHOI</dc:creator>
    <dc:date>2025-05-13T01:24:40Z</dc:date>
    <item>
      <title>Build Error with KM256SW3PHMET_R4_0_0: Fatal Error[Lp049] Related to __iar_data_init3</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-Error-with-KM256SW3PHMET-R4-0-0-Fatal-Error-Lp049-Related/m-p/2095821#M67538</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I downloaded and installed the Three-Phase Power Meter Reference Design Software from the following NXP link:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/three-phase-power-meter-reference-design:THREE-PHASE-POWER-METER" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/three-phase-power-meter-reference-design:THREE-PHASE-POWER-METER&lt;/A&gt;&lt;/P&gt;&lt;P&gt;After installation, I tried to build the project located at:&lt;BR /&gt;C:\freescale\KM256SW3PHMET_R4_0_0\build\iar_7_40\projects\KM256SW3PHMET_R4_0_0&lt;BR /&gt;using IAR Embedded Workbench.&lt;/P&gt;&lt;P&gt;However, I encountered the following error during compilation:&lt;/P&gt;&lt;P&gt;Fatal Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss (adc.o #8)&lt;BR /&gt;I haven't modified any part of the project after installation. Could you please help me understand why this error occurs and how to resolve it?&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Tue, 13 May 2025 01:24:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-Error-with-KM256SW3PHMET-R4-0-0-Fatal-Error-Lp049-Related/m-p/2095821#M67538</guid>
      <dc:creator>MSCHOI</dc:creator>
      <dc:date>2025-05-13T01:24:40Z</dc:date>
    </item>
    <item>
      <title>Re: Build Error with KM256SW3PHMET_R4_0_0: Fatal Error[Lp049] Related to __iar_data_init3</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-Error-with-KM256SW3PHMET-R4-0-0-Fatal-Error-Lp049-Related/m-p/2097724#M67544</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250374"&gt;@MSCHOI&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post and sorry for the late reply.&lt;/P&gt;
&lt;P&gt;This might be related to the inconsistency of IAR versions. The software package uses IAR 7_40. What is the IAR version you are using?&lt;/P&gt;
&lt;P&gt;You can also refer to the following links:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetic-M-Bare-metal-ADC-example-code-linker-errors/m-p/574537" target="_blank"&gt;Kinetic M - Bare metal ADC example code linker errors - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Mkm34z256-Fatal-Error-Lp049/m-p/1841104" target="_blank"&gt;Mkm34z256 -Fatal Error[Lp049] - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BRs,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Thu, 15 May 2025 04:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-Error-with-KM256SW3PHMET-R4-0-0-Fatal-Error-Lp049-Related/m-p/2097724#M67544</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2025-05-15T04:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: Build Error with KM256SW3PHMET_R4_0_0: Fatal Error[Lp049] Related to __iar_data_init3</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-Error-with-KM256SW3PHMET-R4-0-0-Fatal-Error-Lp049-Related/m-p/2097755#M67545</link>
      <description>&lt;P&gt;I’m using version 7.80.4.12495.&lt;BR /&gt;I’ll try to resolve the error by referring to the links you shared.&lt;BR /&gt;Thank you for your prompt response.&lt;/P&gt;</description>
      <pubDate>Thu, 15 May 2025 05:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-Error-with-KM256SW3PHMET-R4-0-0-Fatal-Error-Lp049-Related/m-p/2097755#M67545</guid>
      <dc:creator>MSCHOI</dc:creator>
      <dc:date>2025-05-15T05:11:38Z</dc:date>
    </item>
  </channel>
</rss>