<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Kinetis MK64FN1M0VLL12 – I2C Bus Lock Issue After Wake from STOP Mode? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK64FN1M0VLL12-I2C-Bus-Lock-Issue-After-Wake-from-STOP/m-p/2074568#M67424</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I’m working with the MK64FN1M0VLL12 MCU and running into a weird issue with the I2C bus after waking up from STOP mode. Occasionally, the I2C communication freezes and the SDA line gets stuck low. I suspect it's a bus lock, but I'm not sure the best way to recover without a full reset.&lt;/P&gt;&lt;P&gt;I'm using KSDK 2.x and FreeRTOS, and the I2C is configured in interrupt mode.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Sat, 05 Apr 2025 10:09:05 GMT</pubDate>
    <dc:creator>werovsee</dc:creator>
    <dc:date>2025-04-05T10:09:05Z</dc:date>
    <item>
      <title>Kinetis MK64FN1M0VLL12 – I2C Bus Lock Issue After Wake from STOP Mode?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK64FN1M0VLL12-I2C-Bus-Lock-Issue-After-Wake-from-STOP/m-p/2074568#M67424</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I’m working with the MK64FN1M0VLL12 MCU and running into a weird issue with the I2C bus after waking up from STOP mode. Occasionally, the I2C communication freezes and the SDA line gets stuck low. I suspect it's a bus lock, but I'm not sure the best way to recover without a full reset.&lt;/P&gt;&lt;P&gt;I'm using KSDK 2.x and FreeRTOS, and the I2C is configured in interrupt mode.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Sat, 05 Apr 2025 10:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK64FN1M0VLL12-I2C-Bus-Lock-Issue-After-Wake-from-STOP/m-p/2074568#M67424</guid>
      <dc:creator>werovsee</dc:creator>
      <dc:date>2025-04-05T10:09:05Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK64FN1M0VLL12 – I2C Bus Lock Issue After Wake from STOP Mode?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK64FN1M0VLL12-I2C-Bus-Lock-Issue-After-Wake-from-STOP/m-p/2074623#M67426</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248978" target="_self"&gt;@werov&lt;/A&gt;&lt;A href="https://www.concretesrichmondva.com/" target="_self"&gt;see&lt;/A&gt;&amp;nbsp;wrote:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hi all,&lt;/P&gt;&lt;P&gt;I’m working with the MK64FN1M0VLL12 MCU and running into a weird issue with the I2C bus after waking up from STOP mode. Occasionally, the I2C communication freezes and the SDA line gets stuck low. I suspect it's a bus lock, but I'm not sure the best way to recover without a full reset.&lt;/P&gt;&lt;P&gt;I'm using KSDK 2.x and FreeRTOS, and the I2C is configured in interrupt mode.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;.....?? anyone&lt;/P&gt;</description>
      <pubDate>Sun, 06 Apr 2025 07:21:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK64FN1M0VLL12-I2C-Bus-Lock-Issue-After-Wake-from-STOP/m-p/2074623#M67426</guid>
      <dc:creator>werovsee</dc:creator>
      <dc:date>2025-04-06T07:21:06Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK64FN1M0VLL12 – I2C Bus Lock Issue After Wake from STOP Mode?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK64FN1M0VLL12-I2C-Bus-Lock-Issue-After-Wake-from-STOP/m-p/2075681#M67428</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248978"&gt;@werovsee&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you using a reference board or a custom board?&lt;/P&gt;
&lt;P&gt;If it's a reference board, what is the SCH Version of the board (there is a label pasted on the back of the board)? And please refer to the &lt;A href="https://www.nxp.com.cn/docs/en/errata/FRDMK64F_ERRATA.pdf" target="_self"&gt;FRDM-K64F Board Errata&lt;/A&gt; to check if it matches the situation.&lt;/P&gt;
&lt;P&gt;If it's a custom board, you can refer to the &lt;A href="https://www.nxp.com.cn/docs/en/errata/Kinetis_K_1N83J.pdf" target="_self"&gt;errata for MK64FN1M0VLL12&lt;/A&gt; and see if the following workaround is effective.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1744082911176.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/331783iF791519536D37661/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1744082911176.png" alt="Celeste_Liu_0-1744082911176.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BRs,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 03:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK64FN1M0VLL12-I2C-Bus-Lock-Issue-After-Wake-from-STOP/m-p/2075681#M67428</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2025-04-08T03:29:04Z</dc:date>
    </item>
  </channel>
</rss>