<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックProblems debugging FRDM-K66F with Seeger J-Link Plus</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-debugging-FRDM-K66F-with-Seeger-J-Link-Plus/m-p/2069362#M67404</link>
    <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I want to use the Seeger J-Link plus to debug the MK66FN2M8VMD18 on my FRDM-K66F evaluation board via the SWD debug interface. This interface consists of two signals SWDIO and SWCLK. Unfortunately your wording used in the schematic&amp;nbsp;SPF-28682_REV B.pdf does not correspond to the standard. There are the signals SWD_SDA_TGTMCU, TRACE_SWO, JTAG_TDO/TRACE_SWO/EZP_DO/FTM0_CH7. Which of these signals correspond to the standard SWD signals. I attached the error report additionally. An experienced user could probably detect the fault.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Mar 2025 09:03:40 GMT</pubDate>
    <dc:creator>ChristofAbt</dc:creator>
    <dc:date>2025-03-27T09:03:40Z</dc:date>
    <item>
      <title>Problems debugging FRDM-K66F with Seeger J-Link Plus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-debugging-FRDM-K66F-with-Seeger-J-Link-Plus/m-p/2069362#M67404</link>
      <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I want to use the Seeger J-Link plus to debug the MK66FN2M8VMD18 on my FRDM-K66F evaluation board via the SWD debug interface. This interface consists of two signals SWDIO and SWCLK. Unfortunately your wording used in the schematic&amp;nbsp;SPF-28682_REV B.pdf does not correspond to the standard. There are the signals SWD_SDA_TGTMCU, TRACE_SWO, JTAG_TDO/TRACE_SWO/EZP_DO/FTM0_CH7. Which of these signals correspond to the standard SWD signals. I attached the error report additionally. An experienced user could probably detect the fault.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Mar 2025 09:03:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-debugging-FRDM-K66F-with-Seeger-J-Link-Plus/m-p/2069362#M67404</guid>
      <dc:creator>ChristofAbt</dc:creator>
      <dc:date>2025-03-27T09:03:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problems debugging FRDM-K66F with Seeger J-Link Plus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-debugging-FRDM-K66F-with-Seeger-J-Link-Plus/m-p/2070556#M67407</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248592"&gt;@ChristofAbt&lt;/a&gt;,&lt;BR /&gt;PTA0 and PTA3 corresponds to SWD standard signals:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Habib_MS_4-1743199757570.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/330339iEBF09839852B507A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Habib_MS_4-1743199757570.png" alt="Habib_MS_4-1743199757570.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;And are used in the SDW connector:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Habib_MS_5-1743199890331.png" style="width: 448px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/330340i2351639088DA4DA2/image-dimensions/448x111?v=v2" width="448" height="111" role="button" title="Habib_MS_5-1743199890331.png" alt="Habib_MS_5-1743199890331.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;These are designed to support JTAG and SWD, also, as mentioned in the chapter 3.2 called "Series and debug adapter (OpenSDAv2.1)" in the &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/general-purpose-mcus/freedom-development-platform-for-kinetis-k66-k65-and-k26-mcus:FRDM-K66F#documentation" target="_self"&gt;Freedom FRDM-K66F Development Platform User’s Guide&lt;/A&gt;. These signals are also brought out to a standard 10-pin (0.05”) Cortex Debug connector (J9). I highly recommend see this chapter in order to obtain more information.&lt;BR /&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
      <pubDate>Fri, 28 Mar 2025 22:12:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-debugging-FRDM-K66F-with-Seeger-J-Link-Plus/m-p/2070556#M67407</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2025-03-28T22:12:49Z</dc:date>
    </item>
    <item>
      <title>Re: Problems debugging FRDM-K66F with Seeger J-Link Plus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-debugging-FRDM-K66F-with-Seeger-J-Link-Plus/m-p/2071029#M67411</link>
      <description>&lt;P&gt;Thanks for the quick reply but please use the naming standards in your schematics.&lt;/P&gt;&lt;P&gt;Best regards Christof&lt;/P&gt;</description>
      <pubDate>Mon, 31 Mar 2025 09:54:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-debugging-FRDM-K66F-with-Seeger-J-Link-Plus/m-p/2071029#M67411</guid>
      <dc:creator>ChristofAbt</dc:creator>
      <dc:date>2025-03-31T09:54:20Z</dc:date>
    </item>
    <item>
      <title>Re: Problems debugging FRDM-K66F with Seeger J-Link Plus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-debugging-FRDM-K66F-with-Seeger-J-Link-Plus/m-p/2071445#M67412</link>
      <description>&lt;P&gt;Hello again &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248592"&gt;@ChristofAbt&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for the feedback, I will share the comments to the hardware design team. So,&amp;nbsp;they can deliberate about the addition of this on a future.&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib.&lt;/P&gt;</description>
      <pubDate>Mon, 31 Mar 2025 21:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-debugging-FRDM-K66F-with-Seeger-J-Link-Plus/m-p/2071445#M67412</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2025-03-31T21:44:09Z</dc:date>
    </item>
  </channel>
</rss>