<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADC Speed in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Speed/m-p/161543#M674</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lothar&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After a POR, all the mcu modules will be clocked at a 20.1 MHz frequency, which is predetermined, once the mcu initializes your code it will set up the modules to the CLK frequency you configured.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding ADCK, it has two ranges:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;≤ 13 bit modes&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 MHz &amp;lt; ADCK &amp;lt; 18 MHz&lt;/P&gt;&lt;P&gt;16 bit modes&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 MHz &amp;lt; ADCK &amp;lt; 12 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Depending which resolution you use it is the ADCK range you can work with.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Nov 2012 18:08:11 GMT</pubDate>
    <dc:creator>apanecatl</dc:creator>
    <dc:date>2012-11-20T18:08:11Z</dc:date>
    <item>
      <title>ADC Speed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Speed/m-p/161542#M673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I' m using a tower modul with a K20 72MHz MCU and i would like to use the ADC.&lt;/P&gt;&lt;P&gt;I've got the following questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CFG2[ADHSC] is used to configure a higher clock input frequency. This will allow&lt;/P&gt;&lt;P&gt;faster overall conversion times. To meet internal ADC timing requirements,&lt;/P&gt;&lt;P&gt;CFG2[ADHSC] adds additional ADCK cycles. Conversions with CFG2[ADHSC]=1 take&lt;/P&gt;&lt;P&gt;two more ADCK cycles. CFG2[ADHSC] must be used when the ADCLK exceeds the&lt;/P&gt;&lt;P&gt;limit for CFG2[ADHSC]=0.&lt;/P&gt;&lt;P&gt;From which ADCK upwards it must be set? I didnt found that in the manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After a reset what is the normal clock speed of everything?&lt;/P&gt;&lt;P&gt;Something like that:&lt;/P&gt;&lt;P&gt;Option 2:&lt;/P&gt;&lt;P&gt;Clock Frequency&lt;/P&gt;&lt;P&gt;Core clock 72 MHz&lt;/P&gt;&lt;P&gt;System clock 72 MHz&lt;/P&gt;&lt;P&gt;Bus clock 36 MHz&lt;/P&gt;&lt;P&gt;FlexBus clock 36 MHz&lt;/P&gt;&lt;P&gt;Flash clock 24 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I right with that? Thanks in advance for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Lothar&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Nov 2012 00:28:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Speed/m-p/161542#M673</guid>
      <dc:creator>lothar</dc:creator>
      <dc:date>2012-11-02T00:28:12Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Speed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Speed/m-p/161543#M674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lothar&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After a POR, all the mcu modules will be clocked at a 20.1 MHz frequency, which is predetermined, once the mcu initializes your code it will set up the modules to the CLK frequency you configured.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding ADCK, it has two ranges:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;≤ 13 bit modes&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 MHz &amp;lt; ADCK &amp;lt; 18 MHz&lt;/P&gt;&lt;P&gt;16 bit modes&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 MHz &amp;lt; ADCK &amp;lt; 12 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Depending which resolution you use it is the ADCK range you can work with.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2012 18:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Speed/m-p/161543#M674</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2012-11-20T18:08:11Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Speed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Speed/m-p/161544#M675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my case the clock is somehow set without doing anything. I guess there is a function start() which is called by default and it sets the OUTDIV1-4 Registers and some other stuff. It makes it like that:&lt;/P&gt;&lt;P&gt;Core clock 72 MHz&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OUTDIV1 = 0&lt;/P&gt;&lt;P&gt;System clock 72 MHz&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OUTDIV1 = 0&lt;/P&gt;&lt;P&gt;Bus clock 36 MHz&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OUTDIV2 = 1&lt;/P&gt;&lt;P&gt;FlexBus clock 36 MHz&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OUTDIV3 = 1&lt;/P&gt;&lt;P&gt;Flash clock 24 MHz&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OUTDIV4 = 2&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;The second information about the ADCK is very useful. But where have you found that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;I searched in the Datasheet and in &lt;/SPAN&gt;Cookbook for SAR ADC Measurements.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2012 09:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Speed/m-p/161544#M675</guid>
      <dc:creator>lothar</dc:creator>
      <dc:date>2012-12-11T09:36:34Z</dc:date>
    </item>
  </channel>
</rss>