<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Real time generation using FRDM KV31 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Real-time-generation-using-FRDM-KV31/m-p/2055828#M67349</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am using the FRDM KV31F evaluation board, which contains the microcontroller MKV31F512VLL12. I'm running the PIT to do interrupt-based functionalities.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I need to get real-time information or real timestamps to bind with the data and send it to another device. Please help me how to get real time stamps.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 05 Mar 2025 00:46:14 GMT</pubDate>
    <dc:creator>J_prakash</dc:creator>
    <dc:date>2025-03-05T00:46:14Z</dc:date>
    <item>
      <title>Real time generation using FRDM KV31</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Real-time-generation-using-FRDM-KV31/m-p/2055828#M67349</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am using the FRDM KV31F evaluation board, which contains the microcontroller MKV31F512VLL12. I'm running the PIT to do interrupt-based functionalities.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I need to get real-time information or real timestamps to bind with the data and send it to another device. Please help me how to get real time stamps.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Mar 2025 00:46:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Real-time-generation-using-FRDM-KV31/m-p/2055828#M67349</guid>
      <dc:creator>J_prakash</dc:creator>
      <dc:date>2025-03-05T00:46:14Z</dc:date>
    </item>
    <item>
      <title>Re: Real time generation using FRDM KV31</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Real-time-generation-using-FRDM-KV31/m-p/2056972#M67356</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247588"&gt;@J_prakash&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;The KV31 does not have an RTC module, so it is unable to achieve real-time timing. If you only want to record the relative change of time, you can use the FTM. Regarding the use of the FTM, you can refer to the relevant demos in the SDK.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2025-03-06 183753.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/326983iEBAE4C7C29620723/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot 2025-03-06 183753.png" alt="Screenshot 2025-03-06 183753.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot 2025-03-06 183753.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you.&lt;/P&gt;
&lt;P&gt;BRs,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Thu, 06 Mar 2025 10:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Real-time-generation-using-FRDM-KV31/m-p/2056972#M67356</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2025-03-06T10:38:55Z</dc:date>
    </item>
  </channel>
</rss>