<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックi need  help in configuring the board kl46z and processor mkl26z256vll4  for landzo car</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-need-help-in-configuring-the-board-kl46z-and-processor/m-p/2054177#M67336</link>
    <description>&lt;P&gt;how can i configure these components using the mkl26z256vll4 processor ?&lt;/P&gt;&lt;P&gt;components on the image&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;servomotor&lt;/LI&gt;&lt;LI&gt;motor driver&lt;/LI&gt;&lt;LI&gt;camera&lt;/LI&gt;&lt;LI&gt;bluetoth module&lt;/LI&gt;&lt;LI&gt;debugger&lt;/LI&gt;&lt;LI&gt;power module ...&lt;/LI&gt;&lt;/OL&gt;</description>
    <pubDate>Sun, 02 Mar 2025 11:40:48 GMT</pubDate>
    <dc:creator>Maico</dc:creator>
    <dc:date>2025-03-02T11:40:48Z</dc:date>
    <item>
      <title>i need  help in configuring the board kl46z and processor mkl26z256vll4  for landzo car</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-need-help-in-configuring-the-board-kl46z-and-processor/m-p/2054177#M67336</link>
      <description>&lt;P&gt;how can i configure these components using the mkl26z256vll4 processor ?&lt;/P&gt;&lt;P&gt;components on the image&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;servomotor&lt;/LI&gt;&lt;LI&gt;motor driver&lt;/LI&gt;&lt;LI&gt;camera&lt;/LI&gt;&lt;LI&gt;bluetoth module&lt;/LI&gt;&lt;LI&gt;debugger&lt;/LI&gt;&lt;LI&gt;power module ...&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Sun, 02 Mar 2025 11:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-need-help-in-configuring-the-board-kl46z-and-processor/m-p/2054177#M67336</guid>
      <dc:creator>Maico</dc:creator>
      <dc:date>2025-03-02T11:40:48Z</dc:date>
    </item>
    <item>
      <title>Re: i need  help in configuring the board kl46z and processor mkl26z256vll4  for landzo car</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-need-help-in-configuring-the-board-kl46z-and-processor/m-p/2055923#M67350</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245553"&gt;@Maico&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;I'll provide you with some useful resources as much as possible.&lt;/P&gt;
&lt;P&gt;Our community has lots of knowledge bases. For example,&amp;nbsp;&lt;A href="https://community.nxp.com/t5/The-NXP-Cup-Technical-Reports/tkb-p/nxp-cup-technical-reports@tkb" target="_blank"&gt;The NXP Cup Technical Reports Knowledge Base - NXP Community&lt;/A&gt;,&amp;nbsp;&lt;A href="https://community.nxp.com/t5/University-Programs-Knowledge/tkb-p/uvp@tkb" target="_blank"&gt;University Programs Knowledge Base - NXP Community&lt;/A&gt;&amp;nbsp;and&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Sensors-Knowledge-Base/tkb-p/sensors@tkb" target="_blank"&gt;Sensors Knowledge Base - NXP Community&lt;/A&gt;&amp;nbsp;.&amp;nbsp;You can find many posts useful for your project in it.&lt;/P&gt;
&lt;P&gt;Please also refer to the following post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/University-Programs-Knowledge/NXP-CUP-2019-20-Support-Material/ta-p/1104379" target="_blank"&gt;NXP CUP 2019/20 Support Material - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Sensors-Knowledge-Base/Freescale-Vibration-Monitoring-Program/ta-p/1118586" target="_blank"&gt;Freescale Vibration Monitoring Program - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-FTF-2016-Training/SMI-N2008-Hands-On-Workshop-Motor-Control/ta-p/1122342" target="_blank"&gt;SMI-N2008 Hands-On Workshop Motor Control - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you.&lt;/P&gt;
&lt;P&gt;BRs,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Mar 2025 04:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-need-help-in-configuring-the-board-kl46z-and-processor/m-p/2055923#M67350</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2025-03-05T04:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: i need  help in configuring the board kl46z and processor mkl26z256vll4  for landzo car</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-need-help-in-configuring-the-board-kl46z-and-processor/m-p/2071632#M67413</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Absolutely! Based on your list, here's a breakdown of the components you've mentioned, and how they generally function within a robotic or embedded system:&lt;/P&gt;&lt;P&gt;Servomotor:&lt;BR /&gt;A type of rotary actuator that allows for precise control of angular position, velocity, and acceleration.&lt;BR /&gt;Used for applications requiring accurate movement, such as robotic joints, camera panning/tilting, and valve control.&lt;BR /&gt;Often includes feedback mechanisms (like encoders) to ensure accurate positioning.&lt;BR /&gt;Motor Driver:&lt;BR /&gt;An electronic circuit that controls the power supplied to a motor.&lt;BR /&gt;It allows a low-power control signal (from a microcontroller, for example) to drive a higher-power motor.&lt;BR /&gt;Essential for controlling the speed and direction of motors.&lt;BR /&gt;It is used to control servomotors, and other kinds of motors.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;&lt;A href="https://www.loweskidsworkshop.com" target="_self"&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FFFFFF"&gt;Lowes Kids Workshop&lt;/FONT&gt;&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 04:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-need-help-in-configuring-the-board-kl46z-and-processor/m-p/2071632#M67413</guid>
      <dc:creator>rusy658</dc:creator>
      <dc:date>2025-04-01T04:07:04Z</dc:date>
    </item>
  </channel>
</rss>