<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Communication between laptop and KL25Z via WiFi using ESP8266 (ESP-01) in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-laptop-and-KL25Z-via-WiFi-using-ESP8266/m-p/2013765#M67072</link>
    <description>&lt;P&gt;I want my laptop to communicate with KL25Z via wifi and ESP8266 is the bridge. my laptop sends information to ESP-01 via wifi and then the ESP-01 sends those data to KL25Z via cable (the reverse direction will work as well, from KL25Z to ESP-01 and to laptop). The communication protocol is UART.&lt;/P&gt;&lt;P&gt;To implement this project, I connected my KL25Z to laptop with its own cable. ESP-01 and KL25Z are connected with jumper wires as:&lt;/P&gt;&lt;P&gt;KL25Z 3.3 V --&amp;gt; ESP-01 VCC&lt;/P&gt;&lt;P&gt;KL25Z 3.3 V --&amp;gt; ESP-01 CH_PD&lt;/P&gt;&lt;P&gt;KL25Z GND --&amp;gt; ESP-01 GND&lt;/P&gt;&lt;P&gt;KL25Z TX --&amp;gt; ESP-01 RX&lt;/P&gt;&lt;P&gt;KL25Z RX --&amp;gt; ESP-01 TX&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My problem is to program these boards. It's said we can prgram ESP-01 with USB-to-serial driver or external MCU (which in my case is KL25Z). I'd appreciate your help if you answer following question:&lt;/P&gt;&lt;P&gt;1- Is my connections correct now?&lt;/P&gt;&lt;P&gt;2- How should I program ESP-01 using my KL25Z board? should I first configure the UART between laptop and KL25Z, and configure ESP-01 using that path?&lt;/P&gt;&lt;P&gt;3- Also, can someone explain what does RST, GPIO0 and GPIO2 do? Different websites tell different things and all of those are old. My ESP-01 is new and I want to know pulling these pins high and low will do what.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="FRDM-KL25Z" id="FRDM-KL25Z"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 13 Dec 2024 17:31:25 GMT</pubDate>
    <dc:creator>ElectroDesi9n</dc:creator>
    <dc:date>2024-12-13T17:31:25Z</dc:date>
    <item>
      <title>Communication between laptop and KL25Z via WiFi using ESP8266 (ESP-01)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-laptop-and-KL25Z-via-WiFi-using-ESP8266/m-p/2013765#M67072</link>
      <description>&lt;P&gt;I want my laptop to communicate with KL25Z via wifi and ESP8266 is the bridge. my laptop sends information to ESP-01 via wifi and then the ESP-01 sends those data to KL25Z via cable (the reverse direction will work as well, from KL25Z to ESP-01 and to laptop). The communication protocol is UART.&lt;/P&gt;&lt;P&gt;To implement this project, I connected my KL25Z to laptop with its own cable. ESP-01 and KL25Z are connected with jumper wires as:&lt;/P&gt;&lt;P&gt;KL25Z 3.3 V --&amp;gt; ESP-01 VCC&lt;/P&gt;&lt;P&gt;KL25Z 3.3 V --&amp;gt; ESP-01 CH_PD&lt;/P&gt;&lt;P&gt;KL25Z GND --&amp;gt; ESP-01 GND&lt;/P&gt;&lt;P&gt;KL25Z TX --&amp;gt; ESP-01 RX&lt;/P&gt;&lt;P&gt;KL25Z RX --&amp;gt; ESP-01 TX&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My problem is to program these boards. It's said we can prgram ESP-01 with USB-to-serial driver or external MCU (which in my case is KL25Z). I'd appreciate your help if you answer following question:&lt;/P&gt;&lt;P&gt;1- Is my connections correct now?&lt;/P&gt;&lt;P&gt;2- How should I program ESP-01 using my KL25Z board? should I first configure the UART between laptop and KL25Z, and configure ESP-01 using that path?&lt;/P&gt;&lt;P&gt;3- Also, can someone explain what does RST, GPIO0 and GPIO2 do? Different websites tell different things and all of those are old. My ESP-01 is new and I want to know pulling these pins high and low will do what.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="FRDM-KL25Z" id="FRDM-KL25Z"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 17:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-laptop-and-KL25Z-via-WiFi-using-ESP8266/m-p/2013765#M67072</guid>
      <dc:creator>ElectroDesi9n</dc:creator>
      <dc:date>2024-12-13T17:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between laptop and KL25Z via WiFi using ESP8266 (ESP-01)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-laptop-and-KL25Z-via-WiFi-using-ESP8266/m-p/2014047#M67075</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This is the EPS8266-01 board.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1734318816855.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/315941i11212689C1C5C752/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1734318816855.png" alt="xiangjun_rong_0-1734318816855.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;DIV id="tinyMceEditorxiangjun_rong_1" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV id="tinyMceEditorxiangjun_rong_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;First of all, I suggest you contact support engineer of ESP8266-01 board for the connection.&lt;/P&gt;
&lt;P&gt;For your connection:&lt;/P&gt;
&lt;P&gt;KL25Z 3.3 V --&amp;gt; ESP-01 VCC&lt;/P&gt;
&lt;P&gt;KL25Z 3.3 V --&amp;gt; ESP-01 CH_PD&lt;/P&gt;
&lt;P&gt;KL25Z GND --&amp;gt; ESP-01 GND&lt;/P&gt;
&lt;P&gt;KL25Z TX --&amp;gt; ESP-01 RX&lt;/P&gt;
&lt;P&gt;KL25Z RX --&amp;gt; ESP-01 TX&lt;/P&gt;
&lt;P&gt;It appears that the GPIO0 should be connected to 3.3V.&lt;/P&gt;
&lt;P&gt;Regarding the connection between FRDM-KL25Z, it is okay to just connect the uart TXD/RXD to the above board.&lt;/P&gt;
&lt;P&gt;Pls download SDK package of FRDM-Kl25Z.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en" target="_blank"&gt;https://mcuxpresso.nxp.com/en&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Dec 2024 03:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-laptop-and-KL25Z-via-WiFi-using-ESP8266/m-p/2014047#M67075</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-12-16T03:21:23Z</dc:date>
    </item>
  </channel>
</rss>