<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How To Read Laptop's Touchpad Movement From KL25Z Board in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-To-Read-Laptop-s-Touchpad-Movement-From-KL25Z-Board/m-p/2010011#M67067</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, I suppose that you want to use PC to read the Touch pad movement on FRDM-KL25Z, the touchpad is connected to FRDM-KL25 instead of PC.&lt;/P&gt;
&lt;P&gt;The KL25 has USB port, the PC USB can function as a host of HID class, the USB of FRDM-KL25 can function as device of HID class and send position of the touchpad in fixed cycle time.&lt;/P&gt;
&lt;P&gt;Pls download SDK package of FRDM-KL25Z from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en" target="_blank"&gt;https://mcuxpresso.nxp.com/en&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;On the PC side software, you can use C# or Python to develop the code, we do not support the firmware on PC side.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 09 Dec 2024 09:42:56 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-12-09T09:42:56Z</dc:date>
    <item>
      <title>How To Read Laptop's Touchpad Movement From KL25Z Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-To-Read-Laptop-s-Touchpad-Movement-From-KL25Z-Board/m-p/2009353#M67064</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to do a project with FRDM-KL25Z board and I was wondering is it possible to read my laptop's touchpad data from the board? Like making the touchpad data as input and the board will do a task if I swipe left, let's say.&lt;/P&gt;&lt;P&gt;If it is possible to do so, I would appreciate your full explaination of requirements and steps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="FRDM-KL25Z" id="FRDM-KL25Z"&gt;&lt;/LI-PRODUCT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Dec 2024 20:11:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-To-Read-Laptop-s-Touchpad-Movement-From-KL25Z-Board/m-p/2009353#M67064</guid>
      <dc:creator>ElectroDesi9n</dc:creator>
      <dc:date>2024-12-06T20:11:24Z</dc:date>
    </item>
    <item>
      <title>Re: How To Read Laptop's Touchpad Movement From KL25Z Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-To-Read-Laptop-s-Touchpad-Movement-From-KL25Z-Board/m-p/2010011#M67067</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, I suppose that you want to use PC to read the Touch pad movement on FRDM-KL25Z, the touchpad is connected to FRDM-KL25 instead of PC.&lt;/P&gt;
&lt;P&gt;The KL25 has USB port, the PC USB can function as a host of HID class, the USB of FRDM-KL25 can function as device of HID class and send position of the touchpad in fixed cycle time.&lt;/P&gt;
&lt;P&gt;Pls download SDK package of FRDM-KL25Z from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en" target="_blank"&gt;https://mcuxpresso.nxp.com/en&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;On the PC side software, you can use C# or Python to develop the code, we do not support the firmware on PC side.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Dec 2024 09:42:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-To-Read-Laptop-s-Touchpad-Movement-From-KL25Z-Board/m-p/2010011#M67067</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-12-09T09:42:56Z</dc:date>
    </item>
  </channel>
</rss>