<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: jumping to application with watchdog timer</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/jumping-to-application-with-watchdog-timer/m-p/1965696#M66822</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229543"&gt;@Prasad_330&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I understand you don't have any problems jumping to the application for the first time, but you can't jump there once the watchdog expires.&lt;/P&gt;
&lt;P&gt;Do you jump there from the ISR() or main()?&lt;/P&gt;
&lt;P&gt;Jumping from the handler mode can cause problems.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Wed, 02 Oct 2024 14:13:27 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2024-10-02T14:13:27Z</dc:date>
    <item>
      <title>jumping to application with watchdog timer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/jumping-to-application-with-watchdog-timer/m-p/1963347#M66810</link>
      <description>&lt;P&gt;&amp;nbsp;I am using S32k324&lt;/P&gt;&lt;P&gt;I have bootloader address - 0x4000&lt;/P&gt;&lt;P&gt;I have application address&amp;nbsp; - 0x50400&lt;/P&gt;&lt;P&gt;I am using the watchdog timer in my application,&amp;nbsp; which generates the interrupt when the window time period is expired. Now when the&amp;nbsp;window time period is expired i wanted the program to be executed from the address 0x50400 is it possible ??&lt;/P&gt;&lt;P&gt;I tried it but i am getting hard fault once i jump back 0x50400.&lt;/P&gt;&lt;P&gt;Plz let me know wat are the other parameter that has to taken care.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Sep 2024 07:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/jumping-to-application-with-watchdog-timer/m-p/1963347#M66810</guid>
      <dc:creator>Prasad_330</dc:creator>
      <dc:date>2024-09-27T07:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: jumping to application with watchdog timer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/jumping-to-application-with-watchdog-timer/m-p/1963350#M66811</link>
      <description>Boot loader address - 0x400000</description>
      <pubDate>Fri, 27 Sep 2024 07:45:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/jumping-to-application-with-watchdog-timer/m-p/1963350#M66811</guid>
      <dc:creator>Prasad_330</dc:creator>
      <dc:date>2024-09-27T07:45:11Z</dc:date>
    </item>
    <item>
      <title>Re: jumping to application with watchdog timer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/jumping-to-application-with-watchdog-timer/m-p/1965696#M66822</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229543"&gt;@Prasad_330&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I understand you don't have any problems jumping to the application for the first time, but you can't jump there once the watchdog expires.&lt;/P&gt;
&lt;P&gt;Do you jump there from the ISR() or main()?&lt;/P&gt;
&lt;P&gt;Jumping from the handler mode can cause problems.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 02 Oct 2024 14:13:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/jumping-to-application-with-watchdog-timer/m-p/1965696#M66822</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-10-02T14:13:27Z</dc:date>
    </item>
  </channel>
</rss>