<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: CAN Rx Matching Process not Working</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Rx-Matching-Process-not-Working/m-p/1950462#M66749</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls refer to the section 50.4.5 Rx Mailboxes Global Mask Register (CANx_RXMGMASK) in RM of KE1xF.&lt;/P&gt;
&lt;P&gt;The&amp;nbsp;CANx_RXMGMASK function for mailbox0~13 if CAN_MCR[IRMQ] bit is asserted,&lt;/P&gt;
&lt;P&gt;Each mask bit masks the corresponding Mailbox filter field:&lt;BR /&gt;&lt;BR /&gt;0 The corresponding bit in the filter is "don’t care."&lt;BR /&gt;1 The corresponding bit in the filter is checked.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1725932730458.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298028i6B35BCA3C55FDD3E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1725932730458.png" alt="xiangjun_rong_0-1725932730458.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;In conclusion, pls set the CANx_RXMGMASK bits, so the RX ID in the mailbox will take effect.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 10 Sep 2024 01:51:22 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-09-10T01:51:22Z</dc:date>
    <item>
      <title>CAN Rx Matching Process not Working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Rx-Matching-Process-not-Working/m-p/1948496#M66743</link>
      <description>&lt;P&gt;I am having a hard time understanding how the matching process works on the CAN peripherals for the KE18F processor when the FIFO is disabled.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I set up the Rx mailbox ID to 0x1A5, then set the CODE field to EMPTY.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would expect that packets with ID 0x1A5 would only show up in the mailbox, but it seems to accept any ID.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've read section 50.5.4 of the reference manual, and it seems pretty straight forward, but it just doesn't seem to work.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 19:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Rx-Matching-Process-not-Working/m-p/1948496#M66743</guid>
      <dc:creator>sean_dvorscak</dc:creator>
      <dc:date>2024-09-05T19:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Rx Matching Process not Working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Rx-Matching-Process-not-Working/m-p/1950462#M66749</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls refer to the section 50.4.5 Rx Mailboxes Global Mask Register (CANx_RXMGMASK) in RM of KE1xF.&lt;/P&gt;
&lt;P&gt;The&amp;nbsp;CANx_RXMGMASK function for mailbox0~13 if CAN_MCR[IRMQ] bit is asserted,&lt;/P&gt;
&lt;P&gt;Each mask bit masks the corresponding Mailbox filter field:&lt;BR /&gt;&lt;BR /&gt;0 The corresponding bit in the filter is "don’t care."&lt;BR /&gt;1 The corresponding bit in the filter is checked.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1725932730458.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298028i6B35BCA3C55FDD3E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1725932730458.png" alt="xiangjun_rong_0-1725932730458.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;In conclusion, pls set the CANx_RXMGMASK bits, so the RX ID in the mailbox will take effect.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Sep 2024 01:51:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-Rx-Matching-Process-not-Working/m-p/1950462#M66749</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-09-10T01:51:22Z</dc:date>
    </item>
  </channel>
</rss>