<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMKE02Z64 UART</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z64-UART/m-p/1918525#M66616</link>
    <description>&lt;P&gt;"While using the MKE02Z64 microprocessor to implement serial port data transmission and reception based on the FRDM-KEXX-Driver-Library-Package routine, I observed that the received data consistently omitted the second byte. For instance, when I transmitted 7E 02 30 32 0D (in HEX) from a PC, the simulated microprocessor consistently received 7E 30 32 0D. Furthermore, for other commands, there was always a missing second byte. Despite thorough investigation, I have been unable to identify the root cause of this issue."&lt;/P&gt;</description>
    <pubDate>Sun, 28 Jul 2024 08:42:30 GMT</pubDate>
    <dc:creator>dec88888888</dc:creator>
    <dc:date>2024-07-28T08:42:30Z</dc:date>
    <item>
      <title>MKE02Z64 UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z64-UART/m-p/1918525#M66616</link>
      <description>&lt;P&gt;"While using the MKE02Z64 microprocessor to implement serial port data transmission and reception based on the FRDM-KEXX-Driver-Library-Package routine, I observed that the received data consistently omitted the second byte. For instance, when I transmitted 7E 02 30 32 0D (in HEX) from a PC, the simulated microprocessor consistently received 7E 30 32 0D. Furthermore, for other commands, there was always a missing second byte. Despite thorough investigation, I have been unable to identify the root cause of this issue."&lt;/P&gt;</description>
      <pubDate>Sun, 28 Jul 2024 08:42:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z64-UART/m-p/1918525#M66616</guid>
      <dc:creator>dec88888888</dc:creator>
      <dc:date>2024-07-28T08:42:30Z</dc:date>
    </item>
    <item>
      <title>Re: MKE02Z64 UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z64-UART/m-p/1919093#M66617</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that the the "0x02" is STX, which is not a displaying character.&lt;/P&gt;
&lt;P&gt;Pls try to change the data such as 0x30,0x31,0x32.... which are 0,1,2,3,4...,&amp;nbsp;Pls try to change the data such as 0x41,0x42,0x43(A,B,C...).&lt;/P&gt;
&lt;P&gt;This is ASCII code:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://wenku.baidu.com/view/9ab6d1acb4daa58da1114a1d.html?fr=aladdin664466&amp;amp;ind=4&amp;amp;hitsid=1&amp;amp;target=%E5%B8%AE%E6%88%91%E5%86%99%E4%B8%80%E7%AF%87%E2%80%9Cascii%E7%A0%81%E8%A1%A8%E2%80%9D&amp;amp;aigcsid=0&amp;amp;qtype=0&amp;amp;lcid=4&amp;amp;queryKey=ascii%E7%A0%81%E8%A1%A8&amp;amp;_wkts_=1722233978237&amp;amp;bdQuery=ascii%E7%A0%81%E8%A1%A8&amp;amp;needWelcomeRecommand=1"&gt;https://wenku.baidu.com/view/9ab6d1acb4daa58da1114a1d.html?fr=aladdin664466&amp;amp;ind=4&amp;amp;hitsid=1&amp;amp;target=%E5%B8%AE%E6%88%91%E5%86%99%E4%B8%80%E7%AF%87%E2%80%9Cascii%E7%A0%81%E8%A1%A8%E2%80%9D&amp;amp;aigcsid=0&amp;amp;qtype=0&amp;amp;lcid=4&amp;amp;queryKey=ascii%E7%A0%81%E8%A1%A8&amp;amp;_wkts_=1722233978237&amp;amp;bdQuery=ascii%E7%A0%81%E8%A1%A8&amp;amp;needWelcomeRecommand=1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jul 2024 06:24:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE02Z64-UART/m-p/1919093#M66617</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-07-29T06:24:37Z</dc:date>
    </item>
  </channel>
</rss>