<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MK53DN512ZCLQ10 and MK53DN512CLQ10 difference</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK53DN512ZCLQ10-and-MK53DN512CLQ10-difference/m-p/1898210#M66502</link>
    <description>&lt;P&gt;Hi Pablo, thanks for your quick reply.&lt;/P&gt;&lt;P&gt;Understood. Thanks for the confirmation! this product is at the end of his life, so i think will be easy if i purchase the old one for a while and then thats it..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 03 Jul 2024 08:57:54 GMT</pubDate>
    <dc:creator>ign</dc:creator>
    <dc:date>2024-07-03T08:57:54Z</dc:date>
    <item>
      <title>MK53DN512ZCLQ10 and MK53DN512CLQ10 difference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK53DN512ZCLQ10-and-MK53DN512CLQ10-difference/m-p/1897496#M66491</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;we have been using since long time kinetis micro&amp;nbsp;MK53DN512&lt;STRONG&gt;Z&lt;/STRONG&gt;CLQ10 without problem.&amp;nbsp;&lt;/P&gt;&lt;P&gt;On last production batch, instead that reference, it has been assembled&amp;nbsp;MK53DN512CLQ10, which only diference is the silicon revision&lt;/P&gt;&lt;P&gt;I can flash the firmware inside but boards does not work at all. So, which are the differences between both?, by datasheet i can not find any...&lt;/P&gt;&lt;P&gt;Will, in theory, the&amp;nbsp;MK53DN512&lt;STRONG&gt;Z&lt;/STRONG&gt;CLQ10 firmware be 100%compatible to&amp;nbsp;MK53DN512CLQ10' including also the flash tool/setup ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks in advanced for your help.&lt;/P&gt;&lt;P&gt;ignacio&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 12:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK53DN512ZCLQ10-and-MK53DN512CLQ10-difference/m-p/1897496#M66491</guid>
      <dc:creator>ign</dc:creator>
      <dc:date>2024-07-02T12:38:26Z</dc:date>
    </item>
    <item>
      <title>Re: MK53DN512ZCLQ10 and MK53DN512CLQ10 difference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK53DN512ZCLQ10-and-MK53DN512CLQ10-difference/m-p/1897725#M66493</link>
      <description>&lt;P&gt;&lt;BR /&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235806"&gt;@ign&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The MK53DN512ZCLQ10 is rev1.x 100MHz silicon while MK53DN512CLQ10 is rev 2.x 100MHz. So they are different.&lt;/P&gt;
&lt;P&gt;That's why the old rev1.x silicon product is not recommended for new design.&lt;/P&gt;
&lt;P&gt;This newer version is not 100% compatible with older version, this because new functionalities are added with the update.&lt;/P&gt;
&lt;P&gt;If you want you can check this by comparing both references manual and header files.&lt;/P&gt;
&lt;P&gt;We recommend you to generate a new project with the MK53DN512CLQ10 in order to have the updated header files.&lt;/P&gt;
&lt;P&gt;An apology for the inconvenience.&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 18:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK53DN512ZCLQ10-and-MK53DN512CLQ10-difference/m-p/1897725#M66493</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2024-07-02T18:41:55Z</dc:date>
    </item>
    <item>
      <title>Re: MK53DN512ZCLQ10 and MK53DN512CLQ10 difference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK53DN512ZCLQ10-and-MK53DN512CLQ10-difference/m-p/1898210#M66502</link>
      <description>&lt;P&gt;Hi Pablo, thanks for your quick reply.&lt;/P&gt;&lt;P&gt;Understood. Thanks for the confirmation! this product is at the end of his life, so i think will be easy if i purchase the old one for a while and then thats it..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 08:57:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK53DN512ZCLQ10-and-MK53DN512CLQ10-difference/m-p/1898210#M66502</guid>
      <dc:creator>ign</dc:creator>
      <dc:date>2024-07-03T08:57:54Z</dc:date>
    </item>
  </channel>
</rss>