<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFRDM-KL25Z with UART0 Polling SDK</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-with-UART0-Polling-SDK/m-p/1896139#M66483</link>
    <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I just purchased the FRDM-KL25Z board, and I am trying to run the UART Polling SDK example with some minor adjustments. The UART example for KL25Z is using UART1 but I am trying to implement it with UART0 (Open SDA). I updated the code(attached) and updated the pins(picture attached) to use UART0 and not UART1. I can build the project fine, but the issue is when I try to debug it by pressing the green button it won't follow through the debug process. It gets stuck. I have also attached a video showing the issue. How can I fix this? Any help is appreciated.&lt;/P&gt;</description>
    <pubDate>Fri, 28 Jun 2024 23:18:35 GMT</pubDate>
    <dc:creator>hvidales</dc:creator>
    <dc:date>2024-06-28T23:18:35Z</dc:date>
    <item>
      <title>FRDM-KL25Z with UART0 Polling SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-with-UART0-Polling-SDK/m-p/1896139#M66483</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I just purchased the FRDM-KL25Z board, and I am trying to run the UART Polling SDK example with some minor adjustments. The UART example for KL25Z is using UART1 but I am trying to implement it with UART0 (Open SDA). I updated the code(attached) and updated the pins(picture attached) to use UART0 and not UART1. I can build the project fine, but the issue is when I try to debug it by pressing the green button it won't follow through the debug process. It gets stuck. I have also attached a video showing the issue. How can I fix this? Any help is appreciated.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 23:18:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-with-UART0-Polling-SDK/m-p/1896139#M66483</guid>
      <dc:creator>hvidales</dc:creator>
      <dc:date>2024-06-28T23:18:35Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z with UART0 Polling SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-with-UART0-Polling-SDK/m-p/1898090#M66499</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212149"&gt;@hvidales&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please check whether enabled PORT clock and configured pin as UART functions.&lt;/P&gt;
&lt;P&gt;If it still can't work, please erase whole chip. Change a now MCUXpresso IDE workspace. Create a new project or import your project. Try to debug again.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 07:22:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-with-UART0-Polling-SDK/m-p/1898090#M66499</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-07-03T07:22:01Z</dc:date>
    </item>
  </channel>
</rss>