<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic For KM34 board can we do on the fly AES decryption? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/For-KM34-board-can-we-do-on-the-fly-AES-decryption/m-p/1893526#M66474</link>
    <description>&lt;P&gt;For KM34 we have internal flash and i want to update my&amp;nbsp; encrypted firmware through bootloader, can we decrypt the firmware using MMCAU and then flash to controller using bootloader to execute the code.&lt;/P&gt;&lt;P&gt;Can i get steps to provide security to firmware using MMCAU.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jun 2024 12:03:21 GMT</pubDate>
    <dc:creator>Bhumika</dc:creator>
    <dc:date>2024-06-25T12:03:21Z</dc:date>
    <item>
      <title>For KM34 board can we do on the fly AES decryption?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/For-KM34-board-can-we-do-on-the-fly-AES-decryption/m-p/1893526#M66474</link>
      <description>&lt;P&gt;For KM34 we have internal flash and i want to update my&amp;nbsp; encrypted firmware through bootloader, can we decrypt the firmware using MMCAU and then flash to controller using bootloader to execute the code.&lt;/P&gt;&lt;P&gt;Can i get steps to provide security to firmware using MMCAU.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 12:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/For-KM34-board-can-we-do-on-the-fly-AES-decryption/m-p/1893526#M66474</guid>
      <dc:creator>Bhumika</dc:creator>
      <dc:date>2024-06-25T12:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: For KM34 board can we do on the fly AES decryption?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/For-KM34-board-can-we-do-on-the-fly-AES-decryption/m-p/1893947#M66478</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It is impossible to encrypt the firmware using MMCAU and and decrypt the firmware on the fly, at the same time execute it.&lt;/P&gt;
&lt;P&gt;If&amp;nbsp; you want to on the fly decrypt /execute the firmware, you have to consider the K8x or LPC546xx.&lt;/P&gt;
&lt;P&gt;For the KM34, the on-chip flash provides the protection by writing the Flash Configuration Field&lt;/P&gt;
&lt;P&gt;For detailed inf, pls refer to section 27.3.1 Flash Configuration Field Description in the RM of KM34.&lt;/P&gt;
&lt;P&gt;After the flash is in security mode, the JTAG port is blocked, user can not access the code in flash via JTAG.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 02:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/For-KM34-board-can-we-do-on-the-fly-AES-decryption/m-p/1893947#M66478</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-06-26T02:44:18Z</dc:date>
    </item>
  </channel>
</rss>