<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: System status register MK20DN5</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-status-register-MK20DN5/m-p/1888554#M66450</link>
    <description>&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;many thanks for the reply. I also have one addition issue: when i check these registers, i always read 0 from them for any reset reasons. Do you know why? Is there some inizialitazion that i have to do before reading the registers?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;AC&lt;/P&gt;</description>
    <pubDate>Mon, 17 Jun 2024 09:13:37 GMT</pubDate>
    <dc:creator>AlessioCalderini</dc:creator>
    <dc:date>2024-06-17T09:13:37Z</dc:date>
    <item>
      <title>System status register MK20DN5</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-status-register-MK20DN5/m-p/1886133#M66433</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;i would like to ask you which is the register used in the micro MK20 family that has to be read for check the cause of the reset.&lt;/P&gt;&lt;P&gt;I tried to search a similar topic but i didn't find anything.&lt;/P&gt;&lt;P&gt;Thanks in advance for a reply, thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;AC&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 12:26:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-status-register-MK20DN5/m-p/1886133#M66433</guid>
      <dc:creator>AlessioCalderini</dc:creator>
      <dc:date>2024-06-12T12:26:01Z</dc:date>
    </item>
    <item>
      <title>Re: System status register MK20DN5</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-status-register-MK20DN5/m-p/1888337#M66447</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls refer to section 13.2.1 System Reset Status Register High (MC_SRSH) and section 13.2.2 System Reset Status Register Low (MC_SRSL) in Reference manual of K20(K20P120M100SF2RM.pdf), the two registers reflect the reset sources.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1718595166145.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284358i1BEC4035CB95495E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1718595166145.png" alt="xiangjun_rong_0-1718595166145.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1718595166145.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 03:37:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-status-register-MK20DN5/m-p/1888337#M66447</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-06-17T03:37:04Z</dc:date>
    </item>
    <item>
      <title>Re: System status register MK20DN5</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-status-register-MK20DN5/m-p/1888554#M66450</link>
      <description>&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;many thanks for the reply. I also have one addition issue: when i check these registers, i always read 0 from them for any reset reasons. Do you know why? Is there some inizialitazion that i have to do before reading the registers?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;AC&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 09:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-status-register-MK20DN5/m-p/1888554#M66450</guid>
      <dc:creator>AlessioCalderini</dc:creator>
      <dc:date>2024-06-17T09:13:37Z</dc:date>
    </item>
  </channel>
</rss>