<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Programming possibility using USB (D+, D-) for QN9080</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1882427#M66423</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for the reply,&lt;BR /&gt;&lt;BR /&gt;Yes, we referred to the ISP process. For this ISP mode, we need to use J-Link. Please let me know if I am wrong. But we have a requirement to flash the application file through USB port (using Micro B cable, Signals: D+, D-) only. We don't want to use J-Link. Is it possible to flash application only through USB port instead of J-Link in ISP mode?&lt;BR /&gt;Or Is there any way to do as per our requirement?&lt;BR /&gt;Please provide the required information.&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jun 2024 06:20:45 GMT</pubDate>
    <dc:creator>James5427</dc:creator>
    <dc:date>2024-06-06T06:20:45Z</dc:date>
    <item>
      <title>Programming possibility using USB (D+, D-) for QN9080</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1881207#M66418</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are working on QN9080 MCU. We had a requirement related to program/.bin file flashing in QN9080.&lt;BR /&gt;Presently we are using J-Link to flash the application. Now, we want use only USB port to program teh MCU.&lt;BR /&gt;Is there any possibility of flashing the application to QN9080 using USB port (D+, D-) signals?&lt;BR /&gt;Could anyone please provide the possibility and the procedure information to meet the requirement?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;Vamshi&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jun 2024 05:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1881207#M66418</guid>
      <dc:creator>James5427</dc:creator>
      <dc:date>2024-06-05T05:59:13Z</dc:date>
    </item>
    <item>
      <title>Re: Programming possibility using USB (D+, D-) for QN9080</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1881688#M66421</link>
      <description>&lt;P&gt;Hello Vamshi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. The QN9080 on-chip Rom contains a bootloader which provides IN-System Programming (ISP) feature.&lt;/P&gt;
&lt;P&gt;Please help me checking section 7 (Boot process) from the &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM11023" target="_blank"&gt;QN908x user manual&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jun 2024 17:58:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1881688#M66421</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2024-06-05T17:58:37Z</dc:date>
    </item>
    <item>
      <title>Re: Programming possibility using USB (D+, D-) for QN9080</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1882427#M66423</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for the reply,&lt;BR /&gt;&lt;BR /&gt;Yes, we referred to the ISP process. For this ISP mode, we need to use J-Link. Please let me know if I am wrong. But we have a requirement to flash the application file through USB port (using Micro B cable, Signals: D+, D-) only. We don't want to use J-Link. Is it possible to flash application only through USB port instead of J-Link in ISP mode?&lt;BR /&gt;Or Is there any way to do as per our requirement?&lt;BR /&gt;Please provide the required information.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jun 2024 06:20:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1882427#M66423</guid>
      <dc:creator>James5427</dc:creator>
      <dc:date>2024-06-06T06:20:45Z</dc:date>
    </item>
    <item>
      <title>Re: Programming possibility using USB (D+, D-) for QN9080</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1883703#M66425</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As mentioned on chapter 7, the QN908x supports ISP via USART, SPI and USB.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The USB interface is implemented on the following pins:&lt;/P&gt;
&lt;UL type="disc"&gt;
&lt;LI&gt;PA26 for positive differential data&lt;/LI&gt;
&lt;LI&gt;PA27 for negative differential data&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jun 2024 15:30:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1883703#M66425</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2024-06-07T15:30:01Z</dc:date>
    </item>
    <item>
      <title>Re: Programming possibility using USB (D+, D-) for QN9080</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1885979#M66430</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Thank you for the help,&lt;BR /&gt;&lt;BR /&gt;It worked for me but before flashing actual .bin file, we need to convert to the format it accepts.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Image editor will do all the necessary things to the .bin file generated by IAR/MCU Expresso IDEs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Download the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup" rel="nofollow noopener noreferrer" target="_blank"&gt;Connectivity QTool&lt;/A&gt;&amp;nbsp;found in the same page as the Image Editor and install it. The installation folder for this tool will contain the&amp;nbsp;&lt;EM&gt;libgcc_s_dw2-1.dll&lt;/EM&gt;, so run the&amp;nbsp;&lt;EM&gt;QN908x_Image_Editor_v1.0.0.exe&amp;nbsp;&lt;/EM&gt;from that location. This will set the format and generate a .bin file.&lt;BR /&gt;&lt;BR /&gt;This converted .bin file can be used to flash to the MCU in ISP mode.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 08:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-possibility-using-USB-D-D-for-QN9080/m-p/1885979#M66430</guid>
      <dc:creator>James5427</dc:creator>
      <dc:date>2024-06-12T08:50:01Z</dc:date>
    </item>
  </channel>
</rss>