<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Use of PMCTRL STOPA bit</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1865349#M66377</link>
    <description>&lt;P&gt;Hi, I do have the same issue, could you please share or contact?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 14 May 2024 10:58:02 GMT</pubDate>
    <dc:creator>ebadia</dc:creator>
    <dc:date>2024-05-14T10:58:02Z</dc:date>
    <item>
      <title>Use of PMCTRL STOPA bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1778157#M65822</link>
      <description>&lt;P&gt;I am running the power_manager demo available with the FRDM-K32L2B3 demo board. Following wake from Normal STOP mode, I see that the SMC_PMCTRL[STOPA] bit is set. From the Reference Manual, this should only occur if entry into STOP mode was &lt;EM&gt;prevented&lt;/EM&gt; by an interrupt:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;When set, this read-only status bit indicates an interrupt occured during the previous stop mode entry sequence, preventing the system from entering that mode. This field is cleared by reset or by hardware at the beginning of any stop mode entry sequence and is set if the sequence was aborted.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;However, I have found that the bit is set after a successful entry into STOP and subsequent wake from STOP back to RUN.&lt;/P&gt;&lt;P&gt;Is this a bug with the hardware? Or perhaps a bug in the fsl_smc &lt;FONT face="courier new,courier"&gt;SMC_SetPowerModeStop()&lt;/FONT&gt; method?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Dec 2023 19:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1778157#M65822</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2023-12-20T19:38:25Z</dc:date>
    </item>
    <item>
      <title>Re: Use of PMCTRL STOPA bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1779865#M65833</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/113456"&gt;@aberger&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your sharing, we have reproduced the issue, will reply you after checking with itnernal.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 26 Dec 2023 06:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1779865#M65833</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-12-26T06:20:01Z</dc:date>
    </item>
    <item>
      <title>Re: Use of PMCTRL STOPA bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1782023#M65863</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/113456"&gt;@aberger&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please do not use this bit, the STOPA bit will asserted whenever STOP mode is exist from any wake up source.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jan 2024 05:25:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1782023#M65863</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-01-03T05:25:43Z</dc:date>
    </item>
    <item>
      <title>Re: Use of PMCTRL STOPA bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1782410#M65872</link>
      <description>&lt;P&gt;OK. Good to know. Since the documentation explicitly states otherwise, it should be updated to reflect the&amp;nbsp; actual operation.&lt;/P&gt;&lt;P&gt;Can you offer an alternative for detecting an aborted stop mode entry sequence? It would be useful to know, so that the code execution can simply try again to enter stop mode.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jan 2024 17:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1782410#M65872</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2024-01-03T17:08:51Z</dc:date>
    </item>
    <item>
      <title>Re: Use of PMCTRL STOPA bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1788554#M65943</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/113456"&gt;@aberger&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;After check, There is no another ways&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;for detecting an aborted stop mode entry sequence.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jan 2024 07:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1788554#M65943</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-01-15T07:13:47Z</dc:date>
    </item>
    <item>
      <title>Re: Use of PMCTRL STOPA bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1865349#M66377</link>
      <description>&lt;P&gt;Hi, I do have the same issue, could you please share or contact?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 10:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-PMCTRL-STOPA-bit/m-p/1865349#M66377</guid>
      <dc:creator>ebadia</dc:creator>
      <dc:date>2024-05-14T10:58:02Z</dc:date>
    </item>
  </channel>
</rss>