<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 I2C Interrupt after 8th Bit</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-Interrupt-after-8th-Bit/m-p/1861449#M66359</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have to set an address for a I2C slave (MCP 4728) connected to my MK22FN1M0...&lt;/P&gt;&lt;P&gt;Therefore i have change the state of another pin between bit 8 and bit 9.&lt;/P&gt;&lt;P&gt;My idea was to use the TCF interrupt with FACK enabled, because datasheet says:&lt;/P&gt;&lt;P&gt;"48.4.6.1 Byte transfer interrupt&lt;BR /&gt;The Transfer Complete Flag (TCF) bit is set at the falling edge of the ninth clock to&lt;BR /&gt;indicate the completion of a byte and acknowledgement transfer. When FACK is enabled,&lt;BR /&gt;TCF is then set at the falling edge of eighth clock to indicate the completion of byte."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I get the Interrupt at the 9th bit, but i cannot move the interrupt to the 8th bit.&lt;/P&gt;&lt;P&gt;Am i missing something?&lt;/P&gt;&lt;P&gt;Is FACK not changing TCF behaviour if not in SMBus receiver mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The behaviour i need is this:&lt;/P&gt;&lt;P&gt;LDAC Pin is on a separate I2C independent GPIO&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MCP4728_set_address.jpg" style="width: 799px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/277741iBE1C390B038A6F5B/image-size/large?v=v2&amp;amp;px=999" role="button" title="MCP4728_set_address.jpg" alt="MCP4728_set_address.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;MCP4728_set_address.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 08 May 2024 12:25:47 GMT</pubDate>
    <dc:creator>Joern</dc:creator>
    <dc:date>2024-05-08T12:25:47Z</dc:date>
    <item>
      <title>I2C Interrupt after 8th Bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-Interrupt-after-8th-Bit/m-p/1861449#M66359</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have to set an address for a I2C slave (MCP 4728) connected to my MK22FN1M0...&lt;/P&gt;&lt;P&gt;Therefore i have change the state of another pin between bit 8 and bit 9.&lt;/P&gt;&lt;P&gt;My idea was to use the TCF interrupt with FACK enabled, because datasheet says:&lt;/P&gt;&lt;P&gt;"48.4.6.1 Byte transfer interrupt&lt;BR /&gt;The Transfer Complete Flag (TCF) bit is set at the falling edge of the ninth clock to&lt;BR /&gt;indicate the completion of a byte and acknowledgement transfer. When FACK is enabled,&lt;BR /&gt;TCF is then set at the falling edge of eighth clock to indicate the completion of byte."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I get the Interrupt at the 9th bit, but i cannot move the interrupt to the 8th bit.&lt;/P&gt;&lt;P&gt;Am i missing something?&lt;/P&gt;&lt;P&gt;Is FACK not changing TCF behaviour if not in SMBus receiver mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The behaviour i need is this:&lt;/P&gt;&lt;P&gt;LDAC Pin is on a separate I2C independent GPIO&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MCP4728_set_address.jpg" style="width: 799px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/277741iBE1C390B038A6F5B/image-size/large?v=v2&amp;amp;px=999" role="button" title="MCP4728_set_address.jpg" alt="MCP4728_set_address.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;MCP4728_set_address.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 May 2024 12:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-Interrupt-after-8th-Bit/m-p/1861449#M66359</guid>
      <dc:creator>Joern</dc:creator>
      <dc:date>2024-05-08T12:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Interrupt after 8th Bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-Interrupt-after-8th-Bit/m-p/1874028#M66399</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;You are correct! FACK does not change TCF behavior if not in SMBus mode.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 21:41:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-Interrupt-after-8th-Bit/m-p/1874028#M66399</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-05-23T21:41:08Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Interrupt after 8th Bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-Interrupt-after-8th-Bit/m-p/1875183#M66401</link>
      <description>&lt;P&gt;Hi Leo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for the reply!&lt;/P&gt;&lt;P&gt;I will check if i can switch to SMBus mode for that period.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a nice one!&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 05:26:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-Interrupt-after-8th-Bit/m-p/1875183#M66401</guid>
      <dc:creator>Joern</dc:creator>
      <dc:date>2024-05-27T05:26:57Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Interrupt after 8th Bit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-Interrupt-after-8th-Bit/m-p/1875751#M66403</link>
      <description>&lt;P&gt;You're welcome, any other questions feel free to continue using our technical support service.&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 21:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-Interrupt-after-8th-Bit/m-p/1875751#M66403</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-05-27T21:32:23Z</dc:date>
    </item>
  </channel>
</rss>