<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K20 variable interrupt handling time</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1854272#M66325</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding the Jitter of interrupt, it is difficult to track down and get the reason.&lt;/P&gt;
&lt;P&gt;Pls try to check the following items.&lt;/P&gt;
&lt;P&gt;1)set the core at 120MHz which can reduce the interrupt latency.&lt;/P&gt;
&lt;P&gt;2)pls try to disable all the other interrupt, just enable pin interrupt, use the simple code in&amp;nbsp; the main() so that the core can jump to ISR without executing the atomic instruction.&lt;/P&gt;
&lt;P&gt;void main(void)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;.....&lt;/P&gt;
&lt;P&gt;while(1)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Thu, 25 Apr 2024 04:02:44 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-04-25T04:02:44Z</dc:date>
    <item>
      <title>K20 variable interrupt handling time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1850908#M66317</link>
      <description>&lt;P&gt;In my application running on a MK20DX256VLK10&amp;nbsp; there are several interrupts.&amp;nbsp; One is a rising edge external interrupt set to maximum priority. The other interrupts are set to medium.&amp;nbsp; Inside the external interrupt is some code (see attached) to set a discrete out, wait then clear the discrete out.&amp;nbsp; What I can see is that the discrete pulse (red) is occurring approx 11.3us after the rising edge signal triggering the interrupt (green) and also that the time varies up to about 4us (location of trailing edge of red pulse).&lt;/P&gt;&lt;P&gt;When the if conditional is uncommented so the code inside the interrupt executes periodically (every 1s) then there is additional variability in the time to service the interrupt.&lt;/P&gt;&lt;P&gt;What is causing the 4us servicing variability?&lt;/P&gt;&lt;P&gt;Why is the interrupt serviced approx 11.3us after the edge input trigger source?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="scopepic.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274782i2F904E98D6A3DEE1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="scopepic.jpg" alt="scopepic.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;scopepic.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Interrupt code.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274783i71977ADD8A01664F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Interrupt code.jpg" alt="Interrupt code.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Interrupt code.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Apr 2024 19:23:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1850908#M66317</guid>
      <dc:creator>fporter</dc:creator>
      <dc:date>2024-04-19T19:23:37Z</dc:date>
    </item>
    <item>
      <title>Re: K20 variable interrupt handling time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1851089#M66318</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls refer to the AN12078.pdf, which focuses on the interrupt latency based on ARM Cortex-Mx core.&lt;/P&gt;
&lt;P&gt;The K20 uses Cortex-M4 core, the i.mxrt10xx uses Cortex-M7 core, they have similar features.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12078.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12078.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 02:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1851089#M66318</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-04-22T02:12:40Z</dc:date>
    </item>
    <item>
      <title>Re: K20 variable interrupt handling time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1852705#M66320</link>
      <description>&lt;P&gt;Thanks for the information.&lt;/P&gt;&lt;P&gt;However I'm most concerned not with interrupt latency but with the &lt;U&gt;execution jitter within the interrupt&lt;/U&gt;.&amp;nbsp; The latency appears to be mostly fixed.&amp;nbsp; &lt;U&gt;The timing jitter setting the discrete output is the problem.&lt;/U&gt;&lt;/P&gt;&lt;P&gt;The requirement is to set the discrete output a specified amount of time (Xus +/- 0.25us) after the rising edge of the green trace.&amp;nbsp; So an event interrupt is triggered on the green rising edge and code to set the discrete out is executed from within the interrupt.&amp;nbsp; However there is significant timing jitter setting this discrete.&lt;/P&gt;&lt;P&gt;How to reduce greatly or eliminate this jitter?&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 21:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1852705#M66320</guid>
      <dc:creator>fporter</dc:creator>
      <dc:date>2024-04-23T21:33:47Z</dc:date>
    </item>
    <item>
      <title>Re: K20 variable interrupt handling time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1852995#M66322</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the interrupt jitter for each pin interrupt, the interrupt latency is dependent on the where the core executes when the interrupt happens. If it executes the code in main or the subroutine, the core will jump to the ISR immediately after pushing the predefined registers to stack. If it executes the code in the other ISR, as you know that cortex-M4 supports nested interrupt, the core will check the priority group bits, if the current interrupt has higher priority,&amp;nbsp; the core will jump to the current ISR after pushing the predefined registers to stack. BTW, if the the core execute the atomic operation, the core will jump to ISR after the current atomic operation has finished.&lt;/P&gt;
&lt;P&gt;In conclusion, pls configure the pin interrupt priority level to 0x00, which is the highest interrupt priority. Set the other module interrupt priority level as for example 0xF0, which is the lowest interrupt priority so that the Port pin interrupt can preempt the other interrupt.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1713929930752.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/275429i68A46F3ECC0B875B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1713929930752.png" alt="xiangjun_rong_0-1713929930752.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1713929930752.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 03:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1852995#M66322</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-04-24T03:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: K20 variable interrupt handling time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1854021#M66324</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It is hard to know for sure what the timing error is.&amp;nbsp; The green trace is the pin input that triggers the interrupt.&amp;nbsp; The pink trace is the pin output set from within the interrupt.&amp;nbsp; So either there is latency jitter of the interrupt being serviced or there is execution jitter within the interrupt.&amp;nbsp; When the original scope shot was taken, the pin input interrupt was already set to highest priority (0x00). All other interrupts are set to medium.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any other things to track down to eliminate the jitter?&amp;nbsp; I would think it should be possible to have the pin output set a fixed amount of time from the pin input.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 22:59:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1854021#M66324</guid>
      <dc:creator>fporter</dc:creator>
      <dc:date>2024-04-24T22:59:19Z</dc:date>
    </item>
    <item>
      <title>Re: K20 variable interrupt handling time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1854272#M66325</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding the Jitter of interrupt, it is difficult to track down and get the reason.&lt;/P&gt;
&lt;P&gt;Pls try to check the following items.&lt;/P&gt;
&lt;P&gt;1)set the core at 120MHz which can reduce the interrupt latency.&lt;/P&gt;
&lt;P&gt;2)pls try to disable all the other interrupt, just enable pin interrupt, use the simple code in&amp;nbsp; the main() so that the core can jump to ISR without executing the atomic instruction.&lt;/P&gt;
&lt;P&gt;void main(void)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;.....&lt;/P&gt;
&lt;P&gt;while(1)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;__asm("nop");&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 25 Apr 2024 04:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1854272#M66325</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-04-25T04:02:44Z</dc:date>
    </item>
    <item>
      <title>Re: K20 variable interrupt handling time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1857858#M66336</link>
      <description>&lt;P&gt;Is there another way using the CPU peripherals that this objective could be achieved without depending on a software interrupt routine?&lt;/P&gt;&lt;P&gt;Can a timer be initialized to be enabled on the rising edge of a pin input (green trace) and then trigger a pin output (pink trace) or ADC conversion a specified amount of time (on the order of 1-2us with 100ns precision) after the rising edge pin input?&amp;nbsp; The objective being to time the setting of an output pulse (pink trace) precisely with respect to the input pulse.&lt;/P&gt;</description>
      <pubDate>Tue, 30 Apr 2024 22:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1857858#M66336</guid>
      <dc:creator>fporter</dc:creator>
      <dc:date>2024-04-30T22:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: K20 variable interrupt handling time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1859284#M66348</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that you can use the FTM to implement the scheme. An external trigger signal can be a synchronization signal, which can reinitialize the FTM counter to zero, and the FTM counter counts the tick from zero, the FTM can output PWM signal.,which can be the output signal.&lt;/P&gt;
&lt;P&gt;Pls refer to section 3.11.4. Updating&amp;nbsp; the FTM register with hardware control of AN5142.pdf, which I attached.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 May 2024 02:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-variable-interrupt-handling-time/m-p/1859284#M66348</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-05-06T02:16:19Z</dc:date>
    </item>
  </channel>
</rss>