<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NXP Kinetis bootloader not jumping to user application in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1842056#M66263</link>
    <description>&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;&lt;BR /&gt;any update</description>
    <pubDate>Mon, 08 Apr 2024 06:34:07 GMT</pubDate>
    <dc:creator>arunkannan</dc:creator>
    <dc:date>2024-04-08T06:34:07Z</dc:date>
    <item>
      <title>NXP Kinetis bootloader not jumping to user application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1838072#M66226</link>
      <description>&lt;P&gt;I have flashed NXP Kinetis Bootloader v2.0.0 to&amp;nbsp;MKL16Z128VFT4 and able to send commands and receive response.&lt;/P&gt;&lt;P&gt;Wrote a sample LED program and flashed using write-memory command at 0x9000 to test whether it jumps to user application and also set the same at bootloader_config.h&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#define&lt;/SPAN&gt;&lt;SPAN&gt; BL_APP_VECTOR_TABLE_ADDRESS &lt;/SPAN&gt;&lt;SPAN&gt;0x9000&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;But the bootloader is not jumping to application after reset.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Should I disconnect UART connection to host and try or is there anything else I need to set in code to jump to user application&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Sat, 30 Mar 2024 08:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1838072#M66226</guid>
      <dc:creator>arunkannan</dc:creator>
      <dc:date>2024-03-30T08:02:45Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Kinetis bootloader not jumping to user application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1838945#M66239</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226944"&gt;@arunkannan&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;What about the start address of your user application image?&lt;/P&gt;
&lt;P&gt;The bootloader for kL16, strongly recommend you:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-to-Update-Multiple-Devices-in-a-Network-for/ta-p/1113968" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-to-Update-Multiple-Devices-in-a-Network-for/ta-p/1113968&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This is a simplified version.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 05:28:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1838945#M66239</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-04-02T05:28:07Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Kinetis bootloader not jumping to user application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1839438#M66242</link>
      <description>It is jumping to application in debug mode but in normal mode it is not jumping.&lt;BR /&gt;&lt;BR /&gt;Help with below code.&lt;BR /&gt;&lt;BR /&gt;if (timeoutTicks)&lt;BR /&gt;{&lt;BR /&gt;// Note that we assume that the tick counter won't overflow and wrap back to 0.&lt;BR /&gt;// The timeout value is only up to 65536 milliseconds, and the tick count starts&lt;BR /&gt;// at zero when when inited the microseconds driver just a few moments ago.&lt;BR /&gt;uint64_t elapsedTicks = microseconds_get_ticks() - lastTicks;&lt;BR /&gt;&lt;BR /&gt;// Check if the elapsed time is longer than the timeout.&lt;BR /&gt;if (elapsedTicks &amp;gt;= timeoutTicks)&lt;BR /&gt;{&lt;BR /&gt;#if BL_FEATURE_POWERDOWN&lt;BR /&gt;if (shortTimeout)&lt;BR /&gt;{&lt;BR /&gt;#endif&lt;BR /&gt;// In the case of the typical peripheral timeout, jump to the user application.&lt;BR /&gt;jump_to_application(applicationAddress, stackPointer);</description>
      <pubDate>Tue, 02 Apr 2024 14:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1839438#M66242</guid>
      <dc:creator>arunkannan</dc:creator>
      <dc:date>2024-04-02T14:08:32Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Kinetis bootloader not jumping to user application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1842056#M66263</link>
      <description>&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;&lt;BR /&gt;any update</description>
      <pubDate>Mon, 08 Apr 2024 06:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1842056#M66263</guid>
      <dc:creator>arunkannan</dc:creator>
      <dc:date>2024-04-08T06:34:07Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Kinetis bootloader not jumping to user application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1843200#M66266</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226944"&gt;@arunkannan&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry I'm not understand the " normal mode".&lt;/P&gt;
&lt;P&gt;First you should confirm application works well. Then remap it to 0x9000, build to generate image. Program the image to 0x9000.&amp;nbsp; Debug bootloader to check whether can jump to 0x9000.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Again,&amp;nbsp;&amp;nbsp;&lt;SPAN class="uiOutputText"&gt;strongly recommend you:&lt;/SPAN&gt;&lt;A class="cuf-url forceOutputURL" title="" href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-to-Update-Multiple-Devices-in-a-Network-for/ta-p/1113968" target="_blank" rel="noopener noreferrer" data-value="https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-to-Update-Multiple-Devices-in-a-Network-for/ta-p/1113968"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-to-Update-Multiple-Devices-in-a-Network-for/ta-p/1113968&lt;/A&gt;&lt;SPAN class="uiOutputText"&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Apr 2024 13:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Kinetis-bootloader-not-jumping-to-user-application/m-p/1843200#M66266</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-04-09T13:34:24Z</dc:date>
    </item>
  </channel>
</rss>