<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMkm34z256 -Fatal Error[Lp049]</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mkm34z256-Fatal-Error-Lp049/m-p/1841104#M66255</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working with mkm34z256xxx7 and mkm35z512xxx7 microcontrollers using IAR v9.10.2.&lt;/P&gt;&lt;P&gt;I'm able to build the outfile of&amp;nbsp;mkm mkm35z512xxx7 successfully.&lt;/P&gt;&lt;P&gt;But when I try to build the outfile of&amp;nbsp; mkm34z256xxx7 the below error is shown&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Fatal Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss (irtc.o #8)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;MKMxxZ256_flash.icf is the linker configuration file used for&amp;nbsp;mkm34z256xxx7&amp;nbsp; device.&lt;/P&gt;&lt;P&gt;Why is this error showing?&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;</description>
    <pubDate>Fri, 05 Apr 2024 07:04:02 GMT</pubDate>
    <dc:creator>amal_s</dc:creator>
    <dc:date>2024-04-05T07:04:02Z</dc:date>
    <item>
      <title>Mkm34z256 -Fatal Error[Lp049]</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mkm34z256-Fatal-Error-Lp049/m-p/1841104#M66255</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working with mkm34z256xxx7 and mkm35z512xxx7 microcontrollers using IAR v9.10.2.&lt;/P&gt;&lt;P&gt;I'm able to build the outfile of&amp;nbsp;mkm mkm35z512xxx7 successfully.&lt;/P&gt;&lt;P&gt;But when I try to build the outfile of&amp;nbsp; mkm34z256xxx7 the below error is shown&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Fatal Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss (irtc.o #8)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;MKMxxZ256_flash.icf is the linker configuration file used for&amp;nbsp;mkm34z256xxx7&amp;nbsp; device.&lt;/P&gt;&lt;P&gt;Why is this error showing?&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;</description>
      <pubDate>Fri, 05 Apr 2024 07:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mkm34z256-Fatal-Error-Lp049/m-p/1841104#M66255</guid>
      <dc:creator>amal_s</dc:creator>
      <dc:date>2024-04-05T07:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: Mkm34z256 -Fatal Error[Lp049]</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mkm34z256-Fatal-Error-Lp049/m-p/1844680#M66280</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that you can download a package from SDK based on mkm34z256xxx7 from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Pls have a try&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1712802997578.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/273033i1453FF3476AE58F3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1712802997578.png" alt="xiangjun_rong_0-1712802997578.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1712802997578.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Apr 2024 02:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mkm34z256-Fatal-Error-Lp049/m-p/1844680#M66280</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-04-11T02:37:42Z</dc:date>
    </item>
  </channel>
</rss>