<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TWR-K70F120M + TWR-PROTO-ND without TWR-ELEV possible? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-TWR-PROTO-ND-without-TWR-ELEV-possible/m-p/1841047#M66254</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I have a TWR-K70F120M, can I use the prototype board (TWR-PROTO-ND) without the elevators (TWR-ELEV)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I was wanting to see if I could add some simple passive components by connecting one side of the prototype board to one side of the K70 board.&lt;/P&gt;</description>
    <pubDate>Fri, 05 Apr 2024 03:10:54 GMT</pubDate>
    <dc:creator>Keypuncher</dc:creator>
    <dc:date>2024-04-05T03:10:54Z</dc:date>
    <item>
      <title>TWR-K70F120M + TWR-PROTO-ND without TWR-ELEV possible?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-TWR-PROTO-ND-without-TWR-ELEV-possible/m-p/1841047#M66254</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I have a TWR-K70F120M, can I use the prototype board (TWR-PROTO-ND) without the elevators (TWR-ELEV)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I was wanting to see if I could add some simple passive components by connecting one side of the prototype board to one side of the K70 board.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Apr 2024 03:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-TWR-PROTO-ND-without-TWR-ELEV-possible/m-p/1841047#M66254</guid>
      <dc:creator>Keypuncher</dc:creator>
      <dc:date>2024-04-05T03:10:54Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120M + TWR-PROTO-ND without TWR-ELEV possible?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-TWR-PROTO-ND-without-TWR-ELEV-possible/m-p/1841647#M66260</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This is the schematics of TWR-PROTO:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/downloads/en/schematics/SCH-26187.pdf" target="_blank"&gt;https://www.nxp.com.cn/downloads/en/schematics/SCH-26187.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The TWR-ELEV board can connect the primary side signals of TWR-K70F120M to the TWR-PROTO board.&lt;/P&gt;
&lt;P&gt;If you do not want to use TWR-ELEV, pls refer to&amp;nbsp; the schematics of TWR-K70F120M and check if you can connect the signals of TWR-K70F120M to the TWR-PROTO board, in other words, if the signals on TWR-K70F120M board you want to connect to are connected to a connector on the TWR-K70F120M board so that you can use flying cable to connect them. so it is case by case.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;H2 class="message-subject"&gt;&lt;STRONG&gt;&lt;SPAN class="lia-message-read"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/H2&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 07 Apr 2024 03:22:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-TWR-PROTO-ND-without-TWR-ELEV-possible/m-p/1841647#M66260</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-04-07T03:22:01Z</dc:date>
    </item>
  </channel>
</rss>