<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 KEA 64 FOC SINGLE SHUNT</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-64-FOC-SINGLE-SHUNT/m-p/1834158#M66208</link>
    <description>&lt;P&gt;I want to develop a single resistance FOC on the KEA64 . Is it possible?&lt;/P&gt;</description>
    <pubDate>Mon, 25 Mar 2024 02:54:17 GMT</pubDate>
    <dc:creator>LiXiaoQuan</dc:creator>
    <dc:date>2024-03-25T02:54:17Z</dc:date>
    <item>
      <title>KEA 64 FOC SINGLE SHUNT</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-64-FOC-SINGLE-SHUNT/m-p/1834158#M66208</link>
      <description>&lt;P&gt;I want to develop a single resistance FOC on the KEA64 . Is it possible?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Mar 2024 02:54:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-64-FOC-SINGLE-SHUNT/m-p/1834158#M66208</guid>
      <dc:creator>LiXiaoQuan</dc:creator>
      <dc:date>2024-03-25T02:54:17Z</dc:date>
    </item>
    <item>
      <title>Re: KEA 64 FOC SINGLE SHUNT</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-64-FOC-SINGLE-SHUNT/m-p/1838299#M66228</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It is possible to use single shunt resistor and connect the shunt resistor&amp;nbsp; to reconstruct 3 phase current, but it is complex, especially when the state current is small or two PWM signal edge happens synchronously.&lt;/P&gt;
&lt;P&gt;I attach DRM153.pdf, although the AN uses eFlexWM to generate PWM, but it also adapts to FTM which the K64 uses to generate PWM.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 01 Apr 2024 03:25:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-64-FOC-SINGLE-SHUNT/m-p/1838299#M66228</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-04-01T03:25:14Z</dc:date>
    </item>
  </channel>
</rss>