<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: frdm-kw36 no connection to chips debug port</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kw36-no-connection-to-chips-debug-port/m-p/1827462#M66155</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;As you might know, some of the wireless examples put the device into low power mode, in which the debug-related modules are kept static or powered off depending on the low power level and the board may not be found on discovery.&lt;/P&gt;
&lt;P&gt;Could you please confirm if you have tried the following procedure? When trying to flash/debug your application, try to wake up the device by pressing repeatedly SW3/LLWU or Reset button (board) immediately after selecting "Debug" and while target discovery is trying to connect to the device.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you are using a BLE example project, depending on the base project, inside app_preinclude.h you may find some macros related to low-power such as &lt;/SPAN&gt;&lt;SPAN&gt;gAppLowpowerEnabled_d&lt;/SPAN&gt;&lt;SPAN&gt;; please disable (set to 0) this macro. After this, please try flashing/debugging the demo under this configuration.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Also, the Resurrect Kinetis device feature, part of the GUI Flash Tool, may be helpful.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Wed, 13 Mar 2024 19:13:19 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2024-03-13T19:13:19Z</dc:date>
    <item>
      <title>frdm-kw36 no connection to chips debug port</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kw36-no-connection-to-chips-debug-port/m-p/1825452#M66149</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have manage to load, build, and debug some example programs from the&amp;nbsp;SDK_2_2_12_FRDM-KW36 file for the frdm-kw36 board. I even have a program flashed onto the MCU that allows my phone to connect to the chips Bluetooth broadcast. However, I unplugged the board and re-plugged it back in for another example project and I can no longer connect to the chips debug port. I get this error specifically:&amp;nbsp;&lt;/P&gt;&lt;P&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;BR /&gt;============= SCRIPT: kinetisunlock.scp =============&lt;BR /&gt;Kinetis Unlock Script&lt;BR /&gt;Error: Wire Ack Fault - target connected?&lt;BR /&gt;Assert NRESET&lt;BR /&gt;Reset pin state: 00&lt;BR /&gt;Power up Debug&lt;BR /&gt;Error: Wire not connected&lt;BR /&gt;Error: Wire not connected&lt;BR /&gt;No Debug Power&lt;BR /&gt;============= END SCRIPT ============================&lt;BR /&gt;Failed on connect: Ee(42). Could not connect to core.&lt;BR /&gt;No connection to chip's debug port&lt;BR /&gt;(100) Target Connection Failed&lt;BR /&gt;Unable to perform operation!&lt;BR /&gt;Command failed with exit code 1&lt;/P&gt;&lt;P&gt;I'm not sure what to do and have looked through other peoples posts with similar problems without success:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A title="Original URL: https://community.nxp.com/t5/MCUXpresso-General/FRDM-KW36-Wire-ACK-Fault-in-DAP-access/td-p/863513. Click or tap if you trust this link." href="https://nam11.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FMCUXpresso-General%2FFRDM-KW36-Wire-ACK-Fault-in-DAP-access%2Ftd-p%2F863513&amp;amp;data=05%7C02%7Cprentim2%40wwu.edu%7C8ca88a4d86064b9bd80708dc42049354%7Cdc46140ce26f43efb0ae00f257f478ff%7C0%7C0%7C638457834639914523%7CUnknown%7CTWFpbGZsb3d8eyJWIjoiMC4wLjAwMDAiLCJQIjoiV2luMzIiLCJBTiI6Ik1haWwiLCJXVCI6Mn0%3D%7C0%7C%7C%7C&amp;amp;sdata=RJpDkGRTcntDsr6c%2FCqKtgb%2F1FbPS9aqW2gtN8PBnlE%3D&amp;amp;reserved=0" target="_blank" rel="noopener noreferrer"&gt;https://community.nxp.com/t5/MCUXpresso-General/FRDM-KW36-Wire-ACK-Fault-in-DAP-access/td-p/863513&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A title="Original URL: https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-EVK-Failed-on-connect-Ee-42-Could-not-connect-to-core/m-p/1381075. Click or tap if you trust this link." href="https://nam11.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FLPC-Microcontrollers%2FLPC55S16-EVK-Failed-on-connect-Ee-42-Could-not-connect-to-core%2Fm-p%2F1381075&amp;amp;data=05%7C02%7Cprentim2%40wwu.edu%7C8ca88a4d86064b9bd80708dc42049354%7Cdc46140ce26f43efb0ae00f257f478ff%7C0%7C0%7C638457834639925414%7CUnknown%7CTWFpbGZsb3d8eyJWIjoiMC4wLjAwMDAiLCJQIjoiV2luMzIiLCJBTiI6Ik1haWwiLCJXVCI6Mn0%3D%7C0%7C%7C%7C&amp;amp;sdata=h5WKcdDk0zU8Mfx7tdFMiuM2T6Tz7%2BntlzoeaWbNZzY%3D&amp;amp;reserved=0" target="_blank" rel="noopener noreferrer"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-EVK-Failed-on-connect-Ee-42-Could-not-con...&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Anyone have any suggestions? This seems like a common issue.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 19:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kw36-no-connection-to-chips-debug-port/m-p/1825452#M66149</guid>
      <dc:creator>Prentim2</dc:creator>
      <dc:date>2024-03-11T19:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: frdm-kw36 no connection to chips debug port</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kw36-no-connection-to-chips-debug-port/m-p/1827462#M66155</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;As you might know, some of the wireless examples put the device into low power mode, in which the debug-related modules are kept static or powered off depending on the low power level and the board may not be found on discovery.&lt;/P&gt;
&lt;P&gt;Could you please confirm if you have tried the following procedure? When trying to flash/debug your application, try to wake up the device by pressing repeatedly SW3/LLWU or Reset button (board) immediately after selecting "Debug" and while target discovery is trying to connect to the device.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you are using a BLE example project, depending on the base project, inside app_preinclude.h you may find some macros related to low-power such as &lt;/SPAN&gt;&lt;SPAN&gt;gAppLowpowerEnabled_d&lt;/SPAN&gt;&lt;SPAN&gt;; please disable (set to 0) this macro. After this, please try flashing/debugging the demo under this configuration.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Also, the Resurrect Kinetis device feature, part of the GUI Flash Tool, may be helpful.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 19:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kw36-no-connection-to-chips-debug-port/m-p/1827462#M66155</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-03-13T19:13:19Z</dc:date>
    </item>
  </channel>
</rss>