<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Boot pin for Kinetis MKL16Z128VLH4 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Boot-pin-for-Kinetis-MKL16Z128VLH4/m-p/1808859#M66058</link>
    <description>&lt;P&gt;Which is the boot pin for&amp;nbsp;MKL16Z128VLH4 Kinetis KL16 MCU.&lt;/P&gt;&lt;P&gt;I can only see the reset pin in datasheet.&lt;/P&gt;&lt;P&gt;Are reset pin and boot pin the same?&lt;/P&gt;&lt;P&gt;Let us know which is the boot pin?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 15 Feb 2024 04:51:11 GMT</pubDate>
    <dc:creator>arunkannan</dc:creator>
    <dc:date>2024-02-15T04:51:11Z</dc:date>
    <item>
      <title>Boot pin for Kinetis MKL16Z128VLH4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Boot-pin-for-Kinetis-MKL16Z128VLH4/m-p/1808859#M66058</link>
      <description>&lt;P&gt;Which is the boot pin for&amp;nbsp;MKL16Z128VLH4 Kinetis KL16 MCU.&lt;/P&gt;&lt;P&gt;I can only see the reset pin in datasheet.&lt;/P&gt;&lt;P&gt;Are reset pin and boot pin the same?&lt;/P&gt;&lt;P&gt;Let us know which is the boot pin?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 04:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Boot-pin-for-Kinetis-MKL16Z128VLH4/m-p/1808859#M66058</guid>
      <dc:creator>arunkannan</dc:creator>
      <dc:date>2024-02-15T04:51:11Z</dc:date>
    </item>
    <item>
      <title>Re: Boot pin for Kinetis MKL16Z128VLH4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Boot-pin-for-Kinetis-MKL16Z128VLH4/m-p/1811491#M66070</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the Kinetis KL16, there is not regular boot mode, I mean that you can not download application&amp;nbsp; binary to flash via uart, spi...for KL16.&lt;/P&gt;
&lt;P&gt;The KL16 will execute code in flash directly after Reset, but you can write the 0x0_040D(Flash top address) so that you can configure the core clock, enable/disable the Reset pin and NMI pin...&lt;/P&gt;
&lt;P&gt;For detailed inf, pls refer to section 27.3.1 Flash Configuration Field Description and section 6.3.2 FOPT boot options in the RM of Kl16.&lt;/P&gt;
&lt;P&gt;In conclusion, there is Reset pin, there is not BOOT pin.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 06:08:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Boot-pin-for-Kinetis-MKL16Z128VLH4/m-p/1811491#M66070</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-02-20T06:08:40Z</dc:date>
    </item>
  </channel>
</rss>