<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Spi2 dma</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Spi2-dma/m-p/1806113#M66054</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. You are right. DMA request source for SPI2 is Transmit or Receive. There is not a separate source like with SPI0, but you can use it.&lt;/P&gt;
&lt;P&gt;Yes, if your requirement is to use SPI2, you could use another pin for GPIO to trigger DMA.&lt;/P&gt;
&lt;P&gt;Also, maybe this community post might be helpful: &lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-DMA-module-in-Kinetis-Devices/ta-p/1107248" target="_blank"&gt;Using the DMA module in Kinetis Devices - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
    <pubDate>Tue, 13 Feb 2024 20:31:45 GMT</pubDate>
    <dc:creator>Ricardo_Zamora</dc:creator>
    <dc:date>2024-02-13T20:31:45Z</dc:date>
    <item>
      <title>Spi2 dma</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Spi2-dma/m-p/1805604#M66050</link>
      <description>&lt;P&gt;I work with mk64fn1m0xx12&lt;/P&gt;&lt;P&gt;1. SPI2 CAN WORK WITH DMA?&lt;/P&gt;&lt;P&gt;Beacuse thereis is not source for tx and rx to dmamux only tx or rx&lt;/P&gt;&lt;P&gt;2.can i use gpio faling adge to trigger DMA Connected to SPI2.?&lt;/P&gt;&lt;P&gt;ADVICE&lt;/P&gt;&lt;P&gt;THANK&lt;/P&gt;</description>
      <pubDate>Tue, 13 Feb 2024 04:17:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Spi2-dma/m-p/1805604#M66050</guid>
      <dc:creator>Asaf</dc:creator>
      <dc:date>2024-02-13T04:17:37Z</dc:date>
    </item>
    <item>
      <title>Re: Spi2 dma</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Spi2-dma/m-p/1806113#M66054</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. You are right. DMA request source for SPI2 is Transmit or Receive. There is not a separate source like with SPI0, but you can use it.&lt;/P&gt;
&lt;P&gt;Yes, if your requirement is to use SPI2, you could use another pin for GPIO to trigger DMA.&lt;/P&gt;
&lt;P&gt;Also, maybe this community post might be helpful: &lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-DMA-module-in-Kinetis-Devices/ta-p/1107248" target="_blank"&gt;Using the DMA module in Kinetis Devices - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Tue, 13 Feb 2024 20:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Spi2-dma/m-p/1806113#M66054</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2024-02-13T20:31:45Z</dc:date>
    </item>
    <item>
      <title>Re: Spi2 dma</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Spi2-dma/m-p/1806456#M66055</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I configure spi0 to work with dma and it work properly.&lt;/P&gt;&lt;P&gt;I configura spi2 to work with dma diferent channel the first time i send 1byte i get interrupt and the data is ok. The second time i send 24 bytes only the first byte that transmit is correct and the other is not match to what i send and im not get interrupt at the end&lt;/P&gt;&lt;P&gt;Advice&lt;/P&gt;</description>
      <pubDate>Wed, 14 Feb 2024 10:52:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Spi2-dma/m-p/1806456#M66055</guid>
      <dc:creator>Asaf</dc:creator>
      <dc:date>2024-02-14T10:52:15Z</dc:date>
    </item>
  </channel>
</rss>