<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFTM0 Combine PWM</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM0-Combine-PWM/m-p/1795199#M65980</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using FRDM KV31F microcontroller. Is there any limitation of switching frequency in terms of clock sources(BOARD_BootClockHSRUN() or BOARD_BootClockRUN()) of the combine PWM signals?&lt;/P&gt;&lt;P&gt;At switching frequencies above 50 kHZ, sine PWM is not happening.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 25 Jan 2024 07:41:25 GMT</pubDate>
    <dc:creator>JpVenkatesh</dc:creator>
    <dc:date>2024-01-25T07:41:25Z</dc:date>
    <item>
      <title>FTM0 Combine PWM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM0-Combine-PWM/m-p/1795199#M65980</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using FRDM KV31F microcontroller. Is there any limitation of switching frequency in terms of clock sources(BOARD_BootClockHSRUN() or BOARD_BootClockRUN()) of the combine PWM signals?&lt;/P&gt;&lt;P&gt;At switching frequencies above 50 kHZ, sine PWM is not happening.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jan 2024 07:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM0-Combine-PWM/m-p/1795199#M65980</guid>
      <dc:creator>JpVenkatesh</dc:creator>
      <dc:date>2024-01-25T07:41:25Z</dc:date>
    </item>
    <item>
      <title>Re: FTM0 Combine PWM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM0-Combine-PWM/m-p/1798092#M65995</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;The switching frequency limitation on the FTM depends of the source that is clocking the module. It can be the system clock, the fixed frequency clock, or an external clock.&lt;/P&gt;
&lt;P&gt;For the system clock you can consult in &lt;EM&gt;Table 5-1. Clock Summary &lt;/EM&gt;of reference manual.&amp;nbsp;For the fixed frequency, it must not exceed 1/2 of the system clock frequency. And for the external clock source, it must not exceed 1/4 of the system clock frequency.&lt;/P&gt;
&lt;P&gt;Now the FTM outputs an square PWM signal, not sinusoidal. For that you need to focus in setting the correct external circuit to archive it based in the PWM frequency.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jan 2024 22:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM0-Combine-PWM/m-p/1798092#M65995</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-01-30T22:53:09Z</dc:date>
    </item>
  </channel>
</rss>